Results 1 to 3 of 3

Thread: Cameras: State of the Art 01/2014

  1. Cameras: State of the Art 01/2014

    What is the "State of the Art" for FPV cameras for Mech Warfare starting 2014?

    I want to start a discussion regarding the solutions for all levels of sophistication. From hobbyist to full-embedded-systems-nerd. Recipes, links, how-tos, etc, all welcome!

    Since I haven't taken the plunge yet, I don't have much to offer. I can, however, help anyone interested in an opensource, diy, embedded linux recipe. I have just about every embedded linux platform known to man and can offer observations, opinions, and caveats.

  2. #2

    Re: Cameras: State of the Art 01/2014

    I use a 5.8 GHz 200 mW transmitter/receiver combo from HobbyKing, and a small CCD from the same place. Their site is currently down, so no links. Also, HobbyKing -- bleh.
    I also use a 7" 1200x800 pixel display from adafruit: http://www.adafruit.com/products/1033
    (Although the NTSC version for half the price would be sufficient.)

    The idea is to use a Raspberry Pi in my control setup, and use a EZCAP to merge video with digital read-outs: http://www.ebay.com/itm/like/161051656870?lpid=82

    T
    rossen was going to start carrying a ready-matched system of camera, transmitter, receiver, and display, although I haven't yet seen it in the store (maybe I'm just blind, though.)

    My previous solution was an onboard computer, and a USB webcam (I used a Microsoft LifeCam) and sending the data over a custom UDP protocol over WiFi. I had to use the custom protocol to compress the data enough, and to drop frames in times of congestion rather than stalling the display, like all TCP-based camera streaming does.

  3. #3
    Join Date
    Jul 2012
    Location
    Richmond, IN
    Posts
    652
    Rep Power
    46

    Re: Cameras: State of the Art 01/2014

    I use a Raspberry Pi overclocked to 700 MHz with a Xbox Live Vision webcam using Mjpg-Streamer to host a webpage for it to stream the video.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Robogames 2014?
    By Gort in forum Robotics General Discussion
    Replies: 6
    Last Post: 02-08-2014, 10:13 AM
  2. Interesting Robomaticon 2014 Mobile Robot Tournament in Warsaw
    By Robomaticon in forum Robotics General Discussion
    Replies: 0
    Last Post: 12-06-2013, 03:34 PM
  3. 2011 MW- State of the Union
    By DresnerRobotics in forum Mech Warfare
    Replies: 21
    Last Post: 04-27-2011, 07:51 PM
  4. 2.4 Ghz FPV cameras
    By javafiend in forum Robotics General Discussion
    Replies: 9
    Last Post: 05-26-2010, 07:43 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •