Page 8 of 31 FirstFirst ... 45678910111218 ... LastLast
Results 71 to 80 of 302

Thread: PhantomX using a Teensy 3.1

  1. #71
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    77

    Re: PhantomX using a Teensy 3.1

    Thanks Kurt! I would place an order too. Would you mind start sharing it on OSH Park too? Well if not, I'm using the files. Btw, what software do you recommend to read the files? I found some online gerber file reader though.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  2. #72

    Re: PhantomX using a Teensy 3.1

    Thanks Kåre,

    I can share it up there, I thought I might wait until I got the batch back and make sure I did not completely ... it up. To order your own from there: http://www.oshpark.com/ you simply click on the getting started button. It will ask for a file, which you should be able to pass it the zip file (you can remove all of the stuff from the sub-directory). The file names in the top directory match their specifications: http://www.oshpark.com/guidelines. I believe they can also use Eagle design files directly, but I use diptrace. For me right now OSHPARK works great. Reasonable turnaround and first class mail took 2 days (free)

    What I don't know is for international people, how well this works or if it would make more sense to order from someone else. Example Seeedstudio is cheaper: http://www.seeedstudio.com/depot/?products_id=835 I have not used them, but have heard others have. I think for this size, for 5 of them it is $9.90+11+ (options for color, finish, ...) and they are shipped direct from China. Thought I might verify the price in a little bit. They have a different naming convention for their gerber layers.

    Forgot to mention, I am currently using a beta update for Diptrace: http://www.diptrace.com/downloads/download-diptrace/
    I think I read on their forum, that the released version can not read the new format... Can convert to their Ascii version and read back into released version if needed.

    For the most part I don't do anything with Gerber files. I do however use a free version of viewmate (http://www.pentalogix.com/viewmate.php) to look at the gerbers with. It also has some code to check out the gerber against a set of rules. I usually double check my output with this, before I produce a board.

    There were earlier versions of diptrace that sometimes during the gerber production would round up or down and I did not have the clearances needed. So I check now. Other than it likes to complain about the silk, there are 4 warnings on soldermask for transistor (which maybe I should have mucked with pattern template for). It is too late for me to do this for my build, but maybe I should do it now and update the zip files.

    Kurt

  3. #73

    Re: PhantomX using a Teensy 3.1

    Did an update that moved the transister pads a little farther apart, which I think is a good thing as I had to pull pretty hard to get the pins through the first time... Ran through the test program and it removed the 4 warnings. May now set up a version of this for Seeedstudio

    Edit: But what I don't know about Seeedstudio is they want an additional file: Drill Drawing: pcbname.TXT
    Not sure what this one is or how to generate from diptrace.
    Attached Files Attached Files
    Last edited by KurtEck; 02-15-2014 at 01:58 PM.

  4. #74

    Re: PhantomX using a Teensy 3.1

    Just sort of an FYI - I made minor mod to file (one of the mounting holes was off by 5mil), Also made a copy of the drill file (.xln -> .txt) as this is the name that Seeedstudio uses.

    For the fun of it, I also ordered 5 from them as I am curious about how well they work.
    The price from them is $20.90 plus $10.84 for shipping. If you order $50 I believe shipping is free anywhere... But may take weeks to arrive. So their price is a little cheaper for 5 ($31.74) versus 3 from OSH Park ($34.65).
    Attached Files Attached Files

  5. #75
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    77

    Re: PhantomX using a Teensy 3.1

    Thanks for the update Kurt!
    I think I'll wait placing the order until you've done some hands on testing. Just to be sure all is ok.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  6. #76

    Re: PhantomX using a Teensy 3.1

    Sounds like a good idea. I need to stop playing with Diptrace :lol: I know that LinuxGuy wanted Arduino Shield capabilities, so I thought I would try to lay one out with it.
    Click image for larger version. 

Name:	Teensyduino-.00001.jpg 
Views:	253 
Size:	75.5 KB 
ID:	5381

    Right now, The board is 3"x2.7". Could maybe squeeze the height down to 2.6...
    In 3d here, the bright yellow connectors are for shields. I have it backwards from normal boards as to make it easy to route the digital signals at the bottom. Bottom 3 pin connectors are the digital. The ones on the outside on Right are the standard analog, plus some additional analog. 2nd row has most of the pins from the bottom of the Teensy. The one on the Third row are the Analog only (3.3v only) IO pins. Stiall have speaker, 5v and 3.3v regulators All of the optional jumpers are on the 2x5 just right of the Teensy. Added one switch and one led...

    Not sure if anyone would be interested in this type of layout? I still need to add some labels and the like if I go any farther.

  7. #77

    Re: PhantomX using a Teensy 3.1

    As per some requests up on Lynxmotion, I did a few updates to the last version:
    Click image for larger version. 

Name:	Teensyduino-.00001.jpg 
Views:	219 
Size:	79.8 KB 
ID:	5382

    Still not sure I will fabricate any of these myself, but just in case, here is also a zip file with all of the gerber/drill files. I ran them also through viewmate program to make sure it did not find any errors as well. It also includes a sub-directory with Diptrace (beta) files as well as excel parts list with part numbers from Digikey
    Attached Files Attached Files

  8. #78

    Re: PhantomX using a Teensy 3.1

    Edit: But what I don't know about Seeedstudio is they want an additional file: Drill Drawing: pcbname
    That's an Excellion drill file. It's very similar to plain G-code, with a list of drill diameters up front.
    Here's an example from a board of mine:

    Code:
    %
    M48
    M72
    T01C0.0197
    T02C0.0276
    T03C0.0350
    T04C0.0354
    T05C0.0394
    T06C0.0866
    %
    T01
    X5075Y11959
    X5189Y11180
    X6439Y10930
    X7339Y11730
    X8239Y12730
    X8439Y10780
    X7889Y10280
    X7389Y10180
    X5939Y8680
    X5889Y7930
    X7089Y7180
    X6789Y6330
    X6089Y6430
    X4839Y5430
    X4589Y4280
    X3839Y4280
    X3089Y4280
    X2389Y6980
    X4339Y7680
    X5039Y9780
    X3139Y11180
    X8539Y6780
    X8139Y5730
    X7339Y4430
    X6789Y5080
    X6589Y4430
    X5839Y4430
    X10039Y2780
    X11039Y1430
    X13589Y2830
    X14689Y1630
    T02
    X4089Y13180
    X15639Y11180
    T03
    X3089Y930
    X3089Y1930
    X4089Y1930
    X4089Y930
    X5089Y930
    X5089Y1930
    X6839Y1930
    X7839Y1930
    X7839Y930
    X6839Y930
    X8839Y930
    X8839Y1930
    X10589Y930
    X11589Y930
    X12589Y930
    X13939Y16630
    X12939Y16630
    X11939Y16630
    T04
    X1089Y8930
    X13605Y12230
    X14589Y12230
    X15573Y12230
    X15573Y14430
    X14589Y14430
    X13605Y14430
    T05
    X15589Y3991
    X15589Y5369
    X15589Y7741
    X15589Y9119
    T06
    X1339Y930
    X11489Y6180
    X11489Y10130
    X5139Y15380
    X1339Y16680
    X15839Y16680
    X15839Y930
    M30

  9. #79

    Re: PhantomX using a Teensy 3.1

    Thanks,

    I finally figured out it is the same file (I am pretty sure) that Osh Park wanted named <Board Name>.xln

    Another thing I wondered about is has anyone played much with having Seed Studio actually assemble the boards for them. If so did you restrict yourself to only/mainly using parts from their Open Parts Library (http://www.seeedstudio.com/wiki/Open_parts_library)?
    For example if you wish to use a 1K resistor, your design should use an 0603 and are you restricted to only use those resistors. Example I want a voltage divider with something like 10K and 40K. They have 10K, but no 40K (actually 10K appears to be the largest...)
    (Personally I don't like using 0603 as they are a pain to hand solder and I have had many go flying )

    Again not sure if I will fabricate myself, but I now a few others who are interested.

    Thanks again

  10. #80

    Re: PhantomX using a Teensy 3.1

    I have used them for the Onyx Fire II (gun control) boards. I had to re-design my board for their OPL library -- if you want just a few copies, they will not mount any non-OPL parts. I ended up having to mount Dynamixel connectors, power MOSFETs, and TVS diode myself as they didn't have suitable parts in the OPL. Also, I had to use multiple resistors for some dividers, which made the board bigger.
    So, the question is really for you: What's more important? Getting everything exactly like you want it, or having someone else do it for you?
    If you use their fabrication service (100+ boards) then they can source and mount parts that are not part of the OPL.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. PhantomX Hexapod Kit
    By SuperMiguel in forum Projects For Request and/or Sale
    Replies: 12
    Last Post: 12-29-2013, 09:36 PM
  2. Question(s) PhantomX AX Quadruped Mark II PhantomX Robot Turret Equipped??
    By hwan we in forum Robotics General Discussion
    Replies: 1
    Last Post: 03-11-2013, 02:09 PM
  3. Question(s) PhantomX Drawings?
    By phil0stine in forum Humanoids, Walkers & Crawlers
    Replies: 2
    Last Post: 01-03-2013, 02:09 PM
  4. For learning: PhantomX Hexapod vs PhantomX Quadruped
    By Leugim in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-26-2012, 08:50 AM
  5. My PhantomX Hexapod
    By Gilrock in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 09-26-2012, 02:23 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •