Results 1 to 4 of 4

Thread: Motor sizing for 4 wheeled robot

  1. Motor sizing for 4 wheeled robot

    Hello all !

    This is my first post here and I would appreciate your help.

    I am trying to find suitable motors for a four wheeled robot and doing the following calculations:-

    Robot Characteristics
    ==============

    weight(w)=50 kg
    wheel diameter(d)=8 inch=0.2032 m ==> wheel radius (r) = 0.1016 m
    required velocity (v) = 1 m/s
    required acceleration (a) = 0.1 m/s^2
    inline angle=0 deg
    no of wheels = 4
    expected efficiency = 0.85 ( 85 % )


    Calculations
    =======

    required force (F) = m x a = 5 N
    required Torque (T) = F x r = 0.508 Nm
    required Torque per wheel (Tw) = T/4 = 0.127 Nm
    required torque for 0.85 efficiency Tw=0.149 Nm ==> Tw_kgf= 0.0152 kgf-m
    required rpm = (V*60)/(pi*D) = 93.989 rpm ==> rps= 1.567 rps

    I have been told by my supervisor that these calculations are not correct.

    I cant figure out what I am doing wrong ...

  2. #2

    Re: Motor sizing for 4 wheeled robot

    At a minimum, you are not compensating for friction (unless that's baked into the 0.85 efficiency factor.)
    Also, you are assuming an absolutely flat floor -- no incline climbing.
    That being said 0.1 m/s/s is a very slow acceleration rate. Are you sure that's what you need?

  3. #3
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,315
    Images
    27
    Rep Power
    279

    Re: Motor sizing for 4 wheeled robot

    If you trust your assumptions, using one of these per wheel would be overkill by an order of magnitude.

    ...but there is little chance you will get 85% system efficiency. Motors alone, maybe 85% efficient if decent quality, but smaller motors tend to be less efficient unless you are willing to pay a very high price. Rolling resistance of wheels, gear train losses, etc. can drop system efficiency quite a bit. Also, there is little chance the ground will ever be completely level, so definitely design for a minimum of 10~15% grade to overcome smaller obstacles (would need ~18N/wheel just to hold position on 15% incline). And I expect you are really going to want to be able to stop the robot a lot faster than 0.1m/s^s for safety, so either brakes or much larger motors.


    I consider the four 17W gear motors powering the lab's ~4kg omni-wheel rover to be significantly underpowered (~26N at each wheel at stall). It was able to get up to ~0.6m/s in a second or two carrying (and driven by) a DARwIn-OP, but have not tested that since the chassis (~2kg) and battery (3kg) upgrades. Fully loaded, it would be well below 50kg and I am not sure it could achieve a pathetic 0.1m/s^2 acceleration.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  4. Re: Motor sizing for 4 wheeled robot

    thanks for the replies ...

    @jwatte ... yes this is my requirement at the moment, friction is being ignored

    @tician ... i only need to make sure my calculations are right at this point

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Replies: 0
    Last Post: 01-29-2013, 07:46 PM
  2. good servos for wheeled robots
    By jwb97a in forum Rovers
    Replies: 3
    Last Post: 03-22-2012, 07:07 AM
  3. The new Arduino Wheeled Robot kit
    By PedroR in forum Rovers
    Replies: 12
    Last Post: 09-04-2009, 01:03 PM
  4. Interesting Small two wheeled robot climbs stairs
    By jes1510 in forum Robotics General Discussion
    Replies: 3
    Last Post: 02-20-2009, 03:27 PM
  5. Replies: 0
    Last Post: 03-18-2008, 11:41 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •