Results 1 to 9 of 9

Thread: affection of payload capability with wider body.

  1. affection of payload capability with wider body.

    i am cutting a new chassis for my phantomx, doing some changes for easier battery acces, mounting of aditional boards and cameras and so on. but, how much will increasing the span of the body reduce payload capability? i am looking to widen the body 48mm between the middle legs. will this have a dramatic effect on payload capability?

  2. #2

    Re: affection of payload capability with wider body.

    The width of the body doesn't matter much when in static rest, although if dynamics make the body be a lever arm, then the change in payload is proportional. So, if the width was 100 mm, and now it's 150mm, you'd lose 33% of payload capability.

    To understand why the body width doesn't matter in static situations, consider children's wooden blocks. You can build two pillars with a long block across them. The torque between the pillars and the top-block will be effectively zero (a "perfect hinge.") Now, consider building an "M" shape with a hinge in the middle -- the torque needed at the center will need to be enough to counteract the weight of the top block, times half the width of that block.

    Here's an illustration:


  3. Re: affection of payload capability with wider body.

    thank you for the response. the body was 200mm, i plan to make it 248. so if i follow your above calculation, that turns out to be ca. 20% lost capability.
    but, in your experiment, the overall length of the unit is constant, i plan to only strech the body itself, and add a 4th servo to the leg, which effectively move the point of contact invard to the body. this will make the contact point of the middle legs only 40mm wider. i am hoping this will even out things, altoutgh very little.
    seems like i will realy strech the limits, with six extra servos for 4th DOF, i add 330g + extra brackets and camera.

  4. #4
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    860
    Images
    25
    Rep Power
    89

    Re: affection of payload capability with wider body.

    Just a note. When I made the phantomX 4dof I did notice a quicker battery drain due to more weight and more servos. Though I'm sure you are already aware. I was getting 10-15 min on the 2,200 mah battery. I ended upgrading to 6,600 mah to compensate.

  5. Re: affection of payload capability with wider body.

    as i am new to robotics, so i will probably have my hex connected to the computer for quick troubleshooting, and use an external powersupply. i have read your thread about your 4 DOF walker, it will be usefull for me.

  6. #6
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    860
    Images
    25
    Rep Power
    89

    Re: affection of payload capability with wider body.

    Quote Originally Posted by Thorbear.H View Post
    use an external powersupply
    Make sure you use one with sufficient amps!

  7. Re: affection of payload capability with wider body.

    kevin: i have ordered a powerfull external supply now. but, as i placed my order late when there were 10% discount, i placed the order quicly, not reading that the bulk pack with ax 12's don't come with the brackets

    so the 4th DOF will have to wait, until i can get more brackets printed.

    anyway, i made a prototype chassis in some thin aluminium i had lying around, and used a bowl for mounting the electronics in several layers. the middle legs are now 49 mm further away, and the length of the body is a bit shorter. i tried to simulate the electronics i will be using by putting a weigth of 540g and walk, and it does so without dificulties. with the bowl and camera, it now looks adorable


  8. #8

    Re: affection of payload capability with wider body.

    It's a steampunk soldier hexapod! :-)

  9. #9
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    279

    Re: affection of payload capability with wider body.

    Quote Originally Posted by jwatte View Post
    It's a steampunk soldier hexapod! :-)
    I think steampunk would require a bit more greasy/rusty carbon steel, exposed copper-alloy, and distressed leather. And I think I've watched Spaceballs (and some dancing crab commercial) too many times, because I had visions of it with small eye-holes cut high on the bowl and/or lifting the 'bowler hat'/'helmet' off its head and starting to dance around with a cane.

    Still freaking awesome, and those are some impressive/expensive looking cameras. VGA resolution at 60+ fps with a global shutter?
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. GM10 robot body
    By Rbotguy in forum Garage Sale
    Replies: 0
    Last Post: 01-20-2011, 09:54 PM
  2. Towards a body-worn wireless arm controller
    By Adrenalynn in forum Project Showcase
    Replies: 59
    Last Post: 01-16-2009, 09:32 PM
  3. Contest Entry Skype Controlled Roboquad with Spy Capability
    By roschler in forum Project Showcase
    Replies: 6
    Last Post: 09-16-2008, 11:08 AM
  4. Bioloid Wireless capability on Bioloid(I am using HUV interface)
    By kbv2842 in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 04-11-2008, 10:17 PM
  5. Robot Body Shell
    By Tymtravler in forum Robotics General Discussion
    Replies: 3
    Last Post: 11-26-2007, 04:51 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •