Page 1 of 2 12 LastLast
Results 1 to 10 of 12

Thread: Dual VNH2SP30 assembly

Hybrid View

Previous Post Previous Post   Next Post Next Post
  1. #1
    Join Date
    Apr 2013
    Location
    Geneva, CH
    Posts
    59
    Rep Power
    21

    Dual VNH2SP30 assembly

    Hi,

    Just received my dual VNH2SP3which I will use to drive AEG motors.

    First time ever soldered capacitors to a PCB I understand the shorter leg marked with the "negative strip indicator" is indeed the negative, but I'm unsure as to which way around to put the legs into the holes.


    Click image for larger version. 

Name:	vnh2sp30.PNG 
Views:	734 
Size:	542.7 KB 
ID:	5359


    There is a round solder pad and a square solder pad per capacitor. I can see a little "+" marked against one of the round pads (left one on image), but checking on internet search I see conflicting indications about whether round/square pad is negative/positive (I don't know if there is a standard???).

    Apologies for this numpty newbie question but grateful for a confirmation, many thanks.

  2. #2
    Join Date
    Feb 2012
    Location
    Sydney, Australia
    Posts
    364
    Rep Power
    33

    Re: Dual VNH2SP30 assembly

    If in doubt, I do a continuity test between the pads and V+/GND. Usually a good chance of one of them being connected in that fashion.

    With that said, I'd probably go with the round pad being positive, given the marking you pointed out. Also, all the ground pins appear to be square, looking at the pads on the left and right edges of the board.
    Last edited by Th232; 02-06-2014 at 04:51 AM.

  3. #3
    Join Date
    Apr 2013
    Location
    Geneva, CH
    Posts
    59
    Rep Power
    21

    Re: Dual VNH2SP30 assembly

    OK so I've put this board together, hooked up power (7v), and nothing.

    I have not hooked up any motors or signal pins, just power to vin and gnd. At the least I had expected a power led.

    Any ideas?

  4. #4

    Re: Dual VNH2SP30 assembly

    The schematic on the Pololu site does not show a power LED:



    Also note that it shows a separate need for VCC vs VBAT. You should probably provide a regulated logic voltage on the VCC pin, in addition to motor power on VBAT.
    Last edited by jwatte; 02-06-2014 at 11:21 AM.

  5. #5

    Re: Dual VNH2SP30 assembly

    The square pad usually means "pin 1," and sometimes, but not always, GND is on "pin 1."
    On for example the Raspberry Pi, pin 1 is VCC and pin 5 is GND.
    The fact that there is a + on the solder mask (white drawings) is good, though; that's what you should be following. If they put a "+" next to a pad that is ground, they'd be almost criminally negligent :-)

    Pololu usually has some good hook-up guides. Do they have one for this controller? I've used exactly the same controller, and it's worked fine for me, but I forget whether it has a power LED or not. It may also have "enable" pins that need to be pulled high or low...

  6. #6
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,282
    Images
    27
    Rep Power
    275

    Re: Dual VNH2SP30 assembly

    Their schematic lists no LEDs except direction indicators when the driver is running.

    In a typical application, the power connections are made on one end of the board, and the control connections are made on the other end. +5 volts must be supplied to the board through the smaller 0.1"-spaced pins; the input voltage is available at those pins as well, but the connection is not intended for currents exceeding a few amps. The diagnostic pins can be left disconnected if you do not want to monitor the fault conditions of the motor drivers. INA and INB control the direction of each motor, and the PWM pins turns the motors on or off.
    Since the LEDs are in parallel with the driver outputs, you should be able to test the LEDs without connecting any motors to the outputs. Just apply the +VMOT and +5V, plus a few logic pins and the LEDs should start lighting up.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  7. #7
    Join Date
    Apr 2013
    Location
    Geneva, CH
    Posts
    59
    Rep Power
    21

    Re: Dual VNH2SP30 assembly

    This really helps and is a little comforting, as today has not been a great one, so fingers crossed I've not ****** it.

    Within the next day or so I will hook it up to a spare arduino as per the wiring setup below (minus motors) to test.

    Cheers fellas.

    Click image for larger version. 

Name:	Arduino vnh2sp30.jpg 
Views:	3778 
Size:	108.6 KB 
ID:	5362

    P.S. Must learn to read schematics and recognise how an L.E.D. (amongst other components) looks!

  8. #8

    Re: Dual VNH2SP30 assembly

    You don't need an Arduino to test it. If you have a breadboard and some jumper wires, you can set a particular pin high or low by just connecting it to GND/+5V.

  9. #9
    Join Date
    Apr 2013
    Location
    Geneva, CH
    Posts
    59
    Rep Power
    21

    Re: Dual VNH2SP30 assembly

    She lives! Just hooked up to Arduino with test sketch below and able to get red/green leds alternating which I imagine signifies on/off for the coded forward/reverse motion if I had a motor connected.

    My software is currently designed to enable firing one or both guns according to selection by "pilot". As I understand it, INA1 and INB1 are set according to the following truth table.


    INA1 INB1
    0 0 Brake to GND
    0 1 CCW
    1 0 CW
    1 1 Brake to VCC

    http://www.pololu.com/file/0J52/vnh2sp30.pdf

    In addition to signal for PWM, and 5V/GND, I have two connections to set INA1 and INB1. So 5 connections in total for 1 gun.


    To add another gun and yet retain independent speed control I imagine I just need to add 1 additional PWM connection - I can share the INA1 and INB1 with INA2 and INB2? Plus 5V and GND can be shared?


    I would also appreciate if someone can explain the practical implication and difference between "brake to gnd" and "brake to vcc".


    Thanks to all who helped.



    int InA1 = 6;
    int InB1 = 7;
    int PWM1 = 3;
    int PWM1_val = 64;


    void setup() {
    Serial.begin(9600);
    pinMode(InA1, OUTPUT);
    pinMode(InB1, OUTPUT);
    pinMode(PWM1, OUTPUT);
    }


    void loop() {
    digitalWrite(InA1, HIGH);
    digitalWrite(InB1, LOW);
    analogWrite(PWM1, PWM1_val);
    delay(500);
    digitalWrite(InA1, LOW);
    digitalWrite(InB1, HIGH);
    delay(500);
    }
    Last edited by Grumpybeard; 02-09-2014 at 11:02 AM.

  10. #10

    Re: Dual VNH2SP30 assembly

    As far as I know, there's not much difference between "brake to GND" and "brake to VCC." Sometimes, braking will generate some EMI, and you may perhaps want that connected to one rail over the other for some reason.

    Note that you don't want to be running the gun motors counterclockwise (backwards.)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Re: Help in design to assembly
    By electronics in forum Mechanics / Construction
    Replies: 2
    Last Post: 05-30-2012, 05:05 PM
  2. Bioloid Premium Humanoid Assembly Instructions
    By california-ken in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 09-11-2011, 02:43 PM
  3. Bioloid Assembly Tip
    By Bushwhackr in forum Humanoids, Walkers & Crawlers
    Replies: 5
    Last Post: 05-25-2011, 02:06 PM
  4. Question(s) Phoenix Assembly
    By TaErog in forum Humanoids, Walkers & Crawlers
    Replies: 6
    Last Post: 06-04-2010, 10:26 PM
  5. How do I use the VNH2SP30 IC?
    By librab103 in forum Robotics General Discussion
    Replies: 2
    Last Post: 09-05-2008, 07:17 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •