Results 1 to 2 of 2

Thread: Common Connector Info and Part Number Dump Thread

  1. #1
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    278

    Post Common Connector Info and Part Number Dump Thread

    Since I'm a data packrat/hoarder...

    Dynamixel servos:
    • AX, DX, EX, MX, and RX series:
    • Molex Spox 5264 plugs/housings
    • Molex Spox 5263 crimp pins
    • Molex Spox 5267 headers
    • XL series:
    • Molex Micro-Latch 51065 plugs/housings
    • Molxe Micro-Latch 50212 crimp pins
    • Molex Micro-Latch 53253 headers


    Robotis Controllers (CM-5/510/530/700/730/900/904):
    • The 4-pin comms connector is JST PH series compatible (no change in series naming between housings, pins, and headers).
    • The 2-pin AA and 1S LiPo battery holder connectors are JST PH series compatible.
    • The Robotis LiPo battery connector is Yeonho 25048HS-02000 and the crimp pins are either Yeonho YT250 or YST250.
    • Replacement fuses are Littlefuse 451/453. The holder+fuse is Littlefuse 154/155. Should be 10A rating, fast acting.
    • The CM-5 used 5mmx20mm 5A glass fuses.
    • The CM-904 has no fuse, or high current connectors (only JST PH connectors rated 2A, so not meant for power distribution to servos).

    XBee:
    • 1x10 strips of 2mm pitch pin headers.
    • From the XBee manual:
      • Samtec P/N: MMS-110-01-L-SV (or equivalent)
      • Century Interconnect P/N: CPRMSL20-D-0-1 (or equivalent)
      • Samtec P/N: SMM-110-02-SM-S

    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    278

    Re: Common Connector Info and Part Number Dump Thread

    HobbyKing:
    • FT951/FT952 5.8GHz FPV transmitters
    • Molex PicoBlade 51021 plugs/housings
    • Molex PicoBlade 50079/50058 crimp pins
    • Molex PicoBlade 53261 right-angle SMD headers
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. UF.L connector Xbee
    By ArduTank in forum Mech Warfare
    Replies: 10
    Last Post: 05-27-2013, 04:07 PM
  2. What is the Fit-PC2 power connector?.
    By DresnerRobotics in forum Robot Computers
    Replies: 3
    Last Post: 11-24-2010, 02:10 PM
  3. Dynamixel connector wire
    By Adam in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 06-02-2010, 11:48 AM
  4. Question(s) RX-64 4-pin connector cables
    By dsahm in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 07-24-2009, 12:26 PM
  5. Question(s) Name this connector...
    By Adrenalynn in forum Mechanics / Construction
    Replies: 4
    Last Post: 05-11-2008, 03:29 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •