Results 1 to 4 of 4

Thread: Wheelchair motor control

  1. Wheelchair motor control

    I am trying to make a motorized wheelchair and i have two wheelchair motors. But i don't know the connections diagram , there are four wires coming out from the motor. Some one plz tell hoe to connect the wires and control the motor. Please help me ....

  2. #2

    Re: Wheelchair motor control

    I don't think anybody can help you there, because you haven't listed the motor part number, and you haven't posted any pictures. How is anyone supposed to know what you have on your own?
    It's likely two of the wires are for the motor itself, and two of the wires are for a safety brake, and thus needs to be applied before the motor can turn.
    But this assumes the motors are DC gear motors. However, they could be DCBL, or ACI motors, in which case the wires would be something else.

  3. Re: Wheelchair motor control

    the manufacture is fracmo, and it is a 24V 10 A 138 rpm motor. This are the details i have

  4. #4
    Join Date
    Apr 2014
    Location
    State College, PA, US
    Posts
    104
    Rep Power
    26

    Re: Wheelchair motor control

    Quote Originally Posted by yadusahron View Post
    the manufacture is fracmo, and it is a 24V 10 A 138 rpm motor. This are the details i have
    Are you planning on using these motors on a traditional wheelchair to make it powered, or to make a robot?

    Right now I've started work on a robot based on a powered wheelchair base. I will not be using any of the electronics. The motor controllers use an odd set of signals and send a brake signal.

    For a robot, I disable the brake.

    i would strongly discourage the use of powered wheelchair motors on a traditional wheelchair. If you're building your own, I can send you the electronics that came with my chair if you can pay the shipping. They really aren't useful if you're building a robot though, unless you really know your way around electronics and deciphering unknown protocols.
    -
    A little learning is a dangerous thing.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Alternative to wheelchair motor for payload of 50kg/110lbs
    By garagelane in forum DYNAMIXEL & Robot Actuators
    Replies: 13
    Last Post: 04-11-2014, 12:26 AM
  2. Question(s) Newbie! Control a 12V DC Motor using 1061 Servo Controller and L298 Dual H-Bridge Motor Driver
    By dmar in forum Arbotix, Microcontrollers, Arduino
    Replies: 10
    Last Post: 09-05-2013, 02:32 PM
  3. Question(s) 24v Wheelchair Motor Wiring Question... HELP!!
    By prosper50 in forum Robotics General Discussion
    Replies: 16
    Last Post: 04-15-2012, 01:21 PM
  4. Question(s) Motor control
    By bodhibuilder in forum DYNAMIXEL & Robot Actuators
    Replies: 13
    Last Post: 07-04-2009, 02:44 AM
  5. Question(s) Motor control
    By sam in forum Rovers
    Replies: 2
    Last Post: 12-21-2008, 12:21 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •