Page 1 of 2 12 LastLast
Results 1 to 10 of 16

Thread: Tracks tracks and more tracks!

  1. #1

    Tracks tracks and more tracks!

    Thought I would grab a thread here at Trossen and show some of the work I've been doing. As you can see I like tracks. Wheels are good but a robot with tracks just looks cool. Plus the tracks offer the go anywhere ability once the robot is out of the garage and out in the real world. I tend to over due the power end of it. 42mm planetary motors are my current favorite and give lots of power for the size robots I build.
    Most of my robots run the Basic Stamp. I've recently discovered the Arbotix and have been really interested in the things it can do. Namely the Dynamixel support. I'd like to swap out the controllers in many of my robots for the Arbotix-m.
    More to come!
    Attached Thumbnails Attached Thumbnails Click image for larger version. 

Name:	Picture 027.jpg 
Views:	301 
Size:	96.7 KB 
ID:	5488   Click image for larger version. 

Name:	Picture 026.jpg 
Views:	273 
Size:	127.7 KB 
ID:	5489   Click image for larger version. 

Name:	trackbot 3.jpg 
Views:	288 
Size:	105.9 KB 
ID:	5490   Click image for larger version. 

Name:	trackbots.jpg 
Views:	305 
Size:	130.0 KB 
ID:	5491   Click image for larger version. 

Name:	bottom side.jpg 
Views:	280 
Size:	128.2 KB 
ID:	5492  

    Click image for larger version. 

Name:	Lego trackbot 2.jpg 
Views:	288 
Size:	125.2 KB 
ID:	5494   Click image for larger version. 

Name:	174.jpg 
Views:	292 
Size:	105.6 KB 
ID:	5495   Click image for larger version. 

Name:	Picture 297.jpg 
Views:	273 
Size:	88.6 KB 
ID:	5496   Click image for larger version. 

Name:	almost done.jpg 
Views:	294 
Size:	116.4 KB 
ID:	5497   Click image for larger version. 

Name:	front drone.jpg 
Views:	281 
Size:	106.3 KB 
ID:	5493  


  2. #2

    Re: Tracks tracks and more tracks!

    More projects!
    Attached Thumbnails Attached Thumbnails Click image for larger version. 

Name:	robot 1.jpg 
Views:	245 
Size:	125.1 KB 
ID:	5498   Click image for larger version. 

Name:	robot 2.jpg 
Views:	260 
Size:	121.9 KB 
ID:	5499   Click image for larger version. 

Name:	robot 5.jpg 
Views:	246 
Size:	117.2 KB 
ID:	5500   Click image for larger version. 

Name:	robot 4.jpg 
Views:	247 
Size:	118.6 KB 
ID:	5501   Click image for larger version. 

Name:	robot 3.jpg 
Views:	251 
Size:	111.2 KB 
ID:	5502  

    Click image for larger version. 

Name:	robot 6.jpg 
Views:	247 
Size:	109.2 KB 
ID:	5503   Click image for larger version. 

Name:	legobot 1.jpg 
Views:	252 
Size:	150.4 KB 
ID:	5504  

  3. #3
    Join Date
    Apr 2014
    Location
    State College, PA, US
    Posts
    104
    Rep Power
    22

    Re: Tracks tracks and more tracks!

    That's a lot of tracks! And a lot of projects. And they all look wonderful, though I suspect that the one in "almost done.jpg" isn't finished yet.

    where do you get your treads? I'm thinking about making some once my printer arrives - I've been told Real Soon Now! Making treads will give me an excuse to make some more smaller bots that use them. I wonder if I could make an anti-mouse-mouse? (We have a slight mouse problem in our house now.)

  4. #4

    Re: Tracks tracks and more tracks!

    So, the one with the 42mm motor and planetary gearhead is the "almost done" version?
    Also: Good to see someone else using a Tormach PCNC :-)

  5. #5
    Join Date
    Apr 2014
    Location
    State College, PA, US
    Posts
    104
    Rep Power
    22

    Re: Tracks tracks and more tracks!

    Might I ask where you get your motors?
    -
    A little learning is a dangerous thing.

  6. #6

    Re: Tracks tracks and more tracks!

    I bought a box full of the 42mm planetary motors from a seller on ebay who purchased them from Superdroids and never used them. I also watch for large lots of Pittman motors on ebay with good useable ratios. My last Pittman motor purchase was just over 30 identical motors.

  7. #7

    Re: Tracks tracks and more tracks!

    Quote Originally Posted by DangerousThing View Post
    That's a lot of tracks! And a lot of projects. And they all look wonderful, though I suspect that the one in "almost done.jpg" isn't finished yet.

    where do you get your treads? I'm thinking about making some once my printer arrives - I've been told Real Soon Now! Making treads will give me an excuse to make some more smaller bots that use them. I wonder if I could make an anti-mouse-mouse? (We have a slight mouse problem in our house now.)
    A mouse hunting robot!! I think I'd like to get involved in designing that robot. lol

  8. #8
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    44

    Re: Tracks tracks and more tracks!

    Does anything small you've tried work particularly well outdoors? Thanks for sharing all that. I've got treads ready to use that I've yet to use for a few years now =-x

  9. #9

    Re: Tracks tracks and more tracks!

    The Lynxmotion tracks work well up to a point. If the robot is very heavy, they leave a bit to be desired. They are injection molded plastic with vulcanized rubber after all. That being said, I've had really good luck with them. The three inch versions are really nice but require you to source 2.5" aluminum standoffs as LM doesn't carry them.

    The snow blower tracks seem really cool also. I've purchased a set along with some 4 pole wheel chair motors to build a bigger bot. Someday I'll get around to that project!
    If you've got a particular design in mind, I'd be glad to help you cnc the plates to make it work.

  10. #10

    Re: Tracks tracks and more tracks!

    Got the new Arbotix-M boards today. Now I just have to choose which bot to install it in.....

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Iv'e got a question about quad tracks and turning
    By ntopper in forum Rovers
    Replies: 6
    Last Post: 08-19-2013, 01:52 PM
  2. Replies: 1
    Last Post: 10-25-2012, 04:57 PM
  3. Rubber tracks for your robot
    By jdolecki in forum Garage Sale
    Replies: 2
    Last Post: 06-09-2012, 10:05 AM
  4. Snow blower tracks
    By jdolecki in forum Project Showcase
    Replies: 1
    Last Post: 10-17-2011, 07:32 AM
  5. Backordered 2" Tracks
    By nagmier in forum Off Topic
    Replies: 2
    Last Post: 04-25-2009, 08:09 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •