Page 2 of 2 FirstFirst 12
Results 11 to 16 of 16

Thread: Tracks tracks and more tracks!

  1. #11

    Re: Tracks tracks and more tracks!

    Quote Originally Posted by jwatte View Post
    So, the one with the 42mm motor and planetary gearhead is the "almost done" version?
    Also: Good to see someone else using a Tormach PCNC :-)
    The bot labeled "almost done" is my version of the tri-track offered by LM. The track side plates are cnc 6061 with laser cut inlays of blue acrylic. The motors are 32mm planetary units. The bot has the text to speech board and speaks various phrases depending on how close an object gets to the Ping sensor mounted in the head. There are three Pololu motor controllers mounted along with a Lipo in the back control box. Two operate the tracks and the third operate the column motor to raise and lower the head. The head is mechanically linked to the drive base so it always stays orientated parallel to the ground (he looks straight ahead when the head raises or lowers).
    The bot is actually complete as you see it in the picture.

    Click image for larger version. 

Name:	photo 2.jpg 
Views:	289 
Size:	109.4 KB 
ID:	5511Click image for larger version. 

Name:	photo 1.jpg 
Views:	312 
Size:	84.4 KB 
ID:	5510
    Last edited by Machine27; 04-13-2014 at 07:07 AM.

  2. #12
    Join Date
    Apr 2014
    Location
    State College, PA, US
    Posts
    104
    Rep Power
    22

    Re: Tracks tracks and more tracks!

    Thank you for those last views. The metal and acrylic combinations are beautifully designed and executed. Also it gives us s view of the bot on the left, and it is honkin' huge!
    -
    A little learning is a dangerous thing.

  3. #13

    Re: Tracks tracks and more tracks!

    More track ideas!
    Attached Thumbnails Attached Thumbnails Click image for larger version. 

Name:	578.jpg 
Views:	256 
Size:	158.8 KB 
ID:	5524   Click image for larger version. 

Name:	589.jpg 
Views:	244 
Size:	102.5 KB 
ID:	5525   Click image for larger version. 

Name:	576.jpg 
Views:	237 
Size:	86.0 KB 
ID:	5526  

  4. #14
    Join Date
    Apr 2014
    Location
    State College, PA, US
    Posts
    104
    Rep Power
    22

    Re: Tracks tracks and more tracks!

    Beautiful metalwork there. I can't wait to see what you'll do with those track-sets.

    I'm assuming that is an arm in the middle picture, though I suppose it could be a tail (the background music for that idea, "Aluminum Dog" brought to you by Tom Smith).
    -
    A little learning is a dangerous thing.

  5. #15

    Re: Tracks tracks and more tracks!

    Lol, I didn't even notice the gripper hadn't been installed yet in that picture. It does kinda look like a tail.

    Thanks for that laugh!

  6. #16

    Re: Tracks tracks and more tracks!

    [QUOTE=DangerousThing;63837]Beautiful metalwork there. I can't wait to see what you'll do with those track-sets.

    I ran a few sets on the cnc. Some were sold on ebay and others are still waiting for a future project.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Iv'e got a question about quad tracks and turning
    By ntopper in forum Rovers
    Replies: 6
    Last Post: 08-19-2013, 01:52 PM
  2. Replies: 1
    Last Post: 10-25-2012, 04:57 PM
  3. Rubber tracks for your robot
    By jdolecki in forum Garage Sale
    Replies: 2
    Last Post: 06-09-2012, 10:05 AM
  4. Snow blower tracks
    By jdolecki in forum Project Showcase
    Replies: 1
    Last Post: 10-17-2011, 07:32 AM
  5. Backordered 2" Tracks
    By nagmier in forum Off Topic
    Replies: 2
    Last Post: 04-25-2009, 08:09 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •