Page 2 of 2 FirstFirst 12
Results 11 to 15 of 15

Thread: Need large flat panels for the sides do a robot

  1. Re: Need large flat panels for the sides do a robot

    Quote Originally Posted by tician View Post
    Don't think I've ever seen polypropylene twinwall used for walls except maybe inside pet cages, sheds, and greenhouses.
    I worked in a office where all the interior walls and workspace divisions were aluminum studs covered with this stuff. Held up well to people leaning against and using it as pin board for notes. Looked pretty cool too.

  2. #12
    Join Date
    Apr 2014
    Location
    State College, PA, US
    Posts
    104
    Rep Power
    26

    Re: Need large flat panels for the sides do a robot

    Do you think that taking two squares and bonding them together with the corrugations at a right angle would work to make them stronger?
    -
    A little learning is a dangerous thing.

  3. #13
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    282

    Re: Need large flat panels for the sides do a robot

    Quote Originally Posted by DangerousThing View Post
    Do you think that taking two squares and bonding them together with the corrugations at a right angle would work to make them stronger?
    Almost certainly. The difficulty is in successfully bonding polypropylene to itself. Polypropylene and Polyethylene are best bonded using heat and do not work really well with many adhesives. Even gorilla glue has warnings about its ineffectiveness with PP and PE.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  4. #14

    Re: Need large flat panels for the sides do a robot

    Scotch-Weld DP-8010 can do it, but application is not kitchen table friendly...

  5. #15
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    282

    Re: Need large flat panels for the sides do a robot

    3M also makes double-sided, and adhesive transfer, tapes with an acrylic adhesive (300LSE) that works well for bonding 'Low Surface Energy' materials like PP and PE plastics and powder-coat paint. Not sure you get the same coverage per cost as the epoxy and the bond is not as strong (cannot hang 240kg from it), but it often has a 2+ year shelf-life and is a bit easier and safer to use on multiple projects. 9274 appears to be among the best bonding with a ~115 Oz./In. peel adhesion at application and increasing a bit with time.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Velostat/Linqstat Target Panels
    By Deimos in forum Mech Warfare
    Replies: 59
    Last Post: 09-22-2014, 11:26 PM
  2. New Scoring Panels
    By Deimos in forum Mech Warfare
    Replies: 54
    Last Post: 03-03-2014, 09:32 PM
  3. Power and servo for large robot
    By zurk in forum Power
    Replies: 4
    Last Post: 05-29-2013, 01:50 PM
  4. Large Mobile Robot Parts
    By MSpurk in forum Garage Sale
    Replies: 0
    Last Post: 01-04-2009, 04:07 PM
  5. 8/8/8 Replaces home security panels.
    By Vaughn in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 06-17-2007, 09:42 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •