Results 1 to 2 of 2

Thread: Motor Controller for wheelchair motors

  1. #1
    Join Date
    Apr 2014
    Location
    State College, PA, US
    Posts
    104
    Rep Power
    21

    Motor Controller for wheelchair motors

    Hi,

    I need to control two wheelchair motors. These are powered by a 25.6 LiFePo4 at a large possible number of amps at stall.

    Is the Orion Robotics RoboClaw 2x30 a reasonable solution for motor control? It has a number of desirable features such as encoder decoding and a number of different input types. It also handles two motors.

    Thanks in advance.
    -
    A little learning is a dangerous thing.

  2. #2

    Re: Motor Controller for wheelchair motors

    If the stall of your motors is on the order of 30 Amps, then that would be a good choice. I'm using RoboClaws (plural) in my rover, although lower-rated ones because I use lower-rated motors.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Where would I get wheel encoders for wheelchair motors?
    By DangerousThing in forum Sensors
    Replies: 3
    Last Post: 09-19-2014, 06:05 AM
  2. Wheelchair motor control
    By yadusahron in forum Off Topic
    Replies: 3
    Last Post: 04-10-2014, 10:54 PM
  3. Sabretooth 2x25 and wheelchair motors
    By shobley in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 09-28-2010, 08:49 PM
  4. Question(s) replacing wheelchair motors for Mutant Shopping Cart Project
    By LUCKY13 in forum Mechanics / Construction
    Replies: 4
    Last Post: 06-21-2010, 08:30 PM
  5. Using wheelchair motors: Is there a solenoid???
    By avayan in forum DYNAMIXEL & Robot Actuators
    Replies: 6
    Last Post: 07-26-2009, 08:20 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •