Results 1 to 5 of 5

Thread: Disparity maps: Not smart enough

  1. #1

    Disparity maps: Not smart enough

    So, while waiting for UPS ground to slowly crawl the Onyx Fire II boards into the Amazon warehouses, I'm turning back to my stereo vision project for my rover.

    Here's a screen shot of two calibration images and the disparity map calculated from them:

    Click image for larger version. 

Name:	disparity-map-2014-05-04.jpg 
Views:	623 
Size:	145.2 KB 
ID:	5530

    Thinking about how disparity maps work, I'm not sure that's actually such a good way to do 3D/depth reconstruction. I want to use this mostly for "navigation" and "obstacle determination," which means that there will be a known ground plane which I could almost hard code (or at least estimate from an IMU.) A better reconstruction algorithm would start out with the theory that there is flat, unobstructed ground ahead of it, and then build up areas of evidence for this theory (passable) and areas of contrary evidence (blocked) based on what it already knows of the calibrated camera project. The current OpenCV methods just use projection to rectify the images, and then goes back to matching pixels to each other along scanlines, which seems dumb.

    Ideas? Suggestions? Are there working algorithms like this implemented somewhere already?

    Hey, what do you know? http://graphics.stanford.edu/~pmerre...truction07.pdf

    Will UrbanScape become open source any time soon? It *is* my tax money paying for it after all...

  2. #2
    Join Date
    Jun 2011
    Location
    USA
    Posts
    547
    Images
    107
    Rep Power
    43

    Re: Disparity maps: Not smart enough

    I got nothing, but the other day I did randomly see your question on OpenCV's self-hosted stack overflow regarding this

    A better reconstruction algorithm would start out with the theory that there is flat, unobstructed ground ahead of it, and then build up areas of evidence for this theory (passable) and areas of contrary evidence (blocked) based on what it already knows of the calibrated camera project.
    I've yet to do any reading on calibration images and disparity maps and stereoscopic-y things. How would you handle the transition from e.g. grass to pavement? Or would you in the Robomagellan case desire to stay on grass, and thus default to treating the pavement as an "obstacle"?

  3. #3

    Re: Disparity maps: Not smart enough

    How would you handle the transition from e.g. grass to pavement?
    So, with stereo, the important part is whether the left and right cameras see the same color for the same projected world coordinate or not. As long as the pavement and the grass is level, the stereo should still get the same view.

    One assumption might be that the ground would have some uneven-ness, so you have to search the image for a "nearby" correlation. The delta distance of that correlation compared to canonical would tell you how much higher/lower that patch is. For 3" grass, that would probably work fine!

  4. #4
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    279

    Re: Disparity maps: Not smart enough

    There was an independent stereo matching and disparity finding library that we briefly experimented with in the lab a few years ago. Unfortunately, we were trying to use multi-megapixel images (full-res from fuji stereo cameras) and it was crapping out on anything more than one megapixel. IIRC, I was thinking it was the feature/reference point detection grid being too small relative to the image size, so it would find too many reference points and rarely be able to match them correctly. Not sure if that particular belief was correct or if the multi-megapixel issue has been fixed since then.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  5. #5

    Re: Disparity maps: Not smart enough

    Hmm. That still looks disparity based. And grayscale, to boot. Also, one second for a megapixel image? I'm looking for 10 Hz at 640x360...

    Rectifying both images in real time takes about 30% of one CPU core right now at 30 Hz. That's using software only on a i5, and it's converting from YUYV to RGB at the same time. I can probably optimize that a little bit. I'm happy to throw one or two CPU cores at the "find stereo" problem.

    I made some progress last night, using my "assume there's a ground plane" algorithm.

    A red/blue visualization of the input data post rectification and ground plane reprojection:

    Click image for larger version. 

Name:	redblue.jpg 
Views:	288 
Size:	18.6 KB 
ID:	5579

    Note that things "in the ground plane" converge; things above that plane diverge.
    I'm considering 2D feature detection/matching to find "true spans" of matches/mismatches, rather than just "color based 1D" like disparity maps do.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. News/Announcement Freescale announces low cost smart robot
    By emgrobotics in forum Robotics General Discussion
    Replies: 0
    Last Post: 05-14-2011, 01:49 AM
  2. RVIZ slow when building maps
    By Atom in forum ROS - Robot Operating System
    Replies: 5
    Last Post: 04-30-2011, 10:40 PM
  3. Project Smart range sensor
    By RobotAtlas in forum Sensors
    Replies: 0
    Last Post: 12-01-2010, 10:21 AM
  4. Just For Fun AX-12 Smart Arm Web Page Control Demo
    By MikeG in forum Robotics General Discussion
    Replies: 28
    Last Post: 10-30-2008, 10:58 PM
  5. Discussion Smart Batteries
    By Matt in forum Power
    Replies: 23
    Last Post: 06-06-2008, 11:28 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •