Results 1 to 6 of 6

Thread: 90 degree joint / miter gears

  1. #1

    90 degree joint / miter gears

    I'd like to mount a motor with a 6 mm D shaft at a 90 degree angle (or 60-90 degrees, really.)
    What's a good solution to transfer the motor power to the wheel? I have one motor per wheel, and need to move the motor out of the hub for space reasons.


    I've looked at places like rushgears.com and sdp-si.com, and all the gears they have are $25 each and up -- and I need 10 of them! (It feels weird to pay more for the 90 degree joint than I paid for motor + encoder + gearbox...)


    There are some plastic gears at sdp-si that are $6 each, but they are 1:2 and 1:2.5 ratio.


    Or is there another choice for a 90 degree coupling than miter gears?

  2. #2
    Join Date
    Sep 2008
    Location
    Toronto, Ontario
    Posts
    171
    Images
    43
    Rep Power
    41

    Re: 90 degree joint / miter gears

    How about a universal joint? I don't know what your options are like for something off the shelf, but I wager you could make something pretty decent.

  3. #3
    Join Date
    Feb 2012
    Location
    Sydney, Australia
    Posts
    364
    Rep Power
    36

    Re: 90 degree joint / miter gears

    I'm not sure what space you do have, but is it possible to just offset the motor by using two normal gears instead of having a 60-90 deg turn?

  4. #4

    Re: 90 degree joint / miter gears

    is it possible to just offset the motor
    I considered that, but couldn't see a way to make it work. The reason I want to move the motor out in the first place is to make more space; the suspension gets in the way in most directions.

    I suppose I could go really far, straight up, and use a chain/belt drive, and suspend the motor straight above the wheel... That would add more sprung weight for the suspension, but maybe that's not so bad.

  5. #5

    Re: 90 degree joint / miter gears

    Would like to help, do you have a 3D design, or something with dimensions jwatte?

  6. #6
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    279

    Re: 90 degree joint / miter gears

    Although it is four months late (and 2+ months since jwatte was last active; it's too quiet now...), recent catching up on the projects of a builder of derpy electric vehicles and robots led me to search for replacement gears for angle grinders and other tools on amazon. Although the metal quality is probably not great and not all listings include size/tooth/shaft specs, you can find helical groove, bevel gear sets for <$10 each. Slipping sanity is making the temptation to build an EV of some sort rather unbearable, and PRS sounds like an entertaining excuse to build a large-ish experimental (robot/human) platform.

    Old post first started in May:
    Since you already have a nice double wishbone suspension design on an off-road robot and electronics friggin' hate dirt and moisture, why not simply mount and seal the motors on the chassis and link them to the wheels with shafts and a pair of u-joints/cv-joints, like a traditional car/truck?

    I've been somewhat working on a large-ish robot chassis similar to the amusing suspension of the 2CV but using belt/roller-chain shielded within the tube of the leading/trailing arms of the suspension. Will have quadrature encoders on the shielded shaft, maybe at the wheel but probably at the arm joint if using timing-belt or roller-chain, and likely add an absolute position encoder to determine arm angle for wheelbase/steering and quadrature encoder compensation calculations if I give the suspension a large range of motion. Definitely going for four wheel steering, and will at least be capable of four wheel drive for the lower unique part count.

    Also, thinking of using the weight of the battery pack sliding inside the chassis to control pressure and fluid flow in fore-aft linked chassis suspension and orientation of electronics 'cabin' (basically mounted to chassis on a u-joint with multiple air springs), to prevent horrible pitching during rapid start/stop. During rapid lateral accelerations, the battery will slide a bit inside the chassis and cause restriction in fluid flow (should stiffen and partly decouple) until the battery velocity better matches the chassis velocity. Might need to add some sort of a correction system to maintain suspension compliance when driving on hills, although the acceleration from gravity on most drivable inclines would be quite a bit less than that experienced during rapid start/stop.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project A modified PhantomX to add another degree of freedon running Phoenix software.
    By KevinO in forum Humanoids, Walkers & Crawlers
    Replies: 44
    Last Post: 02-13-2013, 01:19 PM
  2. Question(s) LaserCut Gears
    By alonso in forum Mechanics / Construction
    Replies: 4
    Last Post: 11-18-2012, 09:20 PM
  3. Question(s) Who Wants To Make Their Own Gears?
    By Steve Garrison in forum Robotics General Discussion
    Replies: 18
    Last Post: 10-17-2008, 12:10 AM
  4. 90 degree output, good speed and torque?
    By Adrenalynn in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 09-08-2008, 02:21 AM
  5. Question(s) Metal Gears for KRS-784ICS KHR-2HV
    By rpedro in forum Mechanics / Construction
    Replies: 4
    Last Post: 08-02-2008, 10:16 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •