Results 1 to 6 of 6

Thread: Mounting 2 Cameras for Stereo Vision

  1. Mounting 2 Cameras for Stereo Vision

    Hi, I'm new to robotics - but fairly excited to start - just wanna get an idea if I can mount 2 of the MS Cameras on a phantom x turret.

    I am not sure what kind of brackets come with it, or if I need additional equipment for that kind of setup. Prefer not to have to resort to duct tapes if I at all possible :P



    http://www.trossenrobotics.com/p/Mic...ot-camera.aspx (X2)

    http://www.trossenrobotics.com/p/pha...ot-turret.aspx

  2. #2

    Re: Mounting 2 Cameras for Stereo Vision

    I believe you need to make some additional kind of bracket for that, but I don't have the turret, so I'm not sure.

    I use two MS cameras for my rover, and use OpenCV to calibrate them for stereo. I made the bracket out of 1 inch square aluminum tubing.


    Click image for larger version. 

Name:	dual-cameras.jpg 
Views:	1213 
Size:	122.2 KB 
ID:	5593

  3. Re: Mounting 2 Cameras for Stereo Vision

    Urk... I rather not be doing any drilling in my apartment... besides I just want to code and spent as little time on hardware as possible.

  4. #4

    Re: Mounting 2 Cameras for Stereo Vision

    Drilling 3mm holes in plastic with a cordless drill is totally apartment compatible :-)
    Although I imagine some JB Weld or other epoxy-like adhesive might also work.
    Fasten the stand-offs in the right pattern on the top of the quad walker, and screw the top of the turret into those stand-offs.

  5. #5
    Join Date
    Apr 2014
    Location
    State College, PA, US
    Posts
    104
    Rep Power
    19

    Re: Mounting 2 Cameras for Stereo Vision

    For multi-camera vision you get the best results if you have a full definition of where all the cameras are. With a bracket, you'll be much more positive as to the exact location of the cameras.
    -
    A little learning is a dangerous thing.

  6. #6

    Re: Mounting 2 Cameras for Stereo Vision

    The main requirement is that the cameras don't move after calibration. As long as you can rigidly fix the cameras, then a bracket, some InstalMorph, or superglue can all achieve the same rigid fixing of the cameras, with varying degree of aesthetics.
    Once the cameras are fixed, you need to run calibration of some sort; typically print out a chessboard pattern and take a bunch of pictures and calculate the camera distortion and projection based on detecting that pattern. OpenCV has functions for this.
    Once calibrated, you can rectify left/right input pictures so the same scanlines represent the same horizontal lines in the world, which simplifies the work of trying to figure out matches vs disparities between the cameras.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Cameras: State of the Art 01/2014
    By coreyfro in forum Mech Warfare
    Replies: 2
    Last Post: 12-26-2013, 10:01 PM
  2. Commercial stereo vision system
    By harena in forum Sensors
    Replies: 0
    Last Post: 12-09-2012, 06:35 AM
  3. libdc1394v2 and stereo camera
    By rob-bot in forum ROS - Robot Operating System
    Replies: 1
    Last Post: 02-24-2011, 08:20 PM
  4. 2.4 Ghz FPV cameras
    By javafiend in forum Robotics General Discussion
    Replies: 9
    Last Post: 05-26-2010, 06:43 AM
  5. News/Announcement Using the Minoru 3D webcam for stereo vision
    By motters in forum Sensors
    Replies: 2
    Last Post: 06-20-2009, 11:35 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •