Page 6 of 6 FirstFirst ... 23456
Results 51 to 59 of 59

Thread: First steps for Super Mega Microbot

  1. #51
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,255
    Images
    27
    Rep Power
    273

    Re: First steps for Super Mega Microbot

    http://www.etotheipiplusone.net/?p=4688

    Onyx is plenty strong enough for full-combat beetleweight robots, so will likely be good enough for MechWarfare as long as you use proper wall thicknesses and infill settings and maybe add fiber if it's really needed. Would even work for the gearboxes if the teeth are large enough. Which reminds me that I still need to get my compound epicyclic gearbox printed - got put on hold a few months ago because of funding issues and my BuildOne is still likely several months away from delivery.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  2. Re: First steps for Super Mega Microbot

    Yeah, I'm not worried about anything getting fractured by BBs with any of the materials, even shapeways nylon. I used Onyx for the legs because they were bearing load over a long lever arm. With at least the setup I have now, they are less rigid than I would like in the lateral dimension. I don't think I want to make them wide enough to achieve the same rigidity in both axes and ridges or webbing aren't really an option because of the link geometry.

  3. #53
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,255
    Images
    27
    Rep Power
    273

    Re: First steps for Super Mega Microbot

    Is the lack of rigidity a bad thing, given you have been making this thing jump about? Elastic elements are a very big deal when dealing with non-trivial masses/velocities and less than smooth motion no matter how nice you think your sensors and control algorithm are. A bit of flex or springiness is better than breaking teeth, snapping bolts, or deforming bearing surfaces.

    Is the bigger issue not "bolting a leg to the face of a gearbox" instead of supporting it on both sides with bearings to prevent it ripping out the output stage of the gearbox?
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  4. Re: First steps for Super Mega Microbot

    In this case the gearbox is actually supported by two separate bearings internally on either side of a planet carrier, so it is plenty rigid and robust to torsional loads. However, the Onyx printed leg when fully extended can deform by +- 4cm laterally even when rigidly mounted on the top. My goal is not to make a series elastic actuator, but instead to have something that is accurately controllable with a high bandwidth while still being highly backdrivable.

    And yes, my mostly non-existent sensors and control algorithms are very nice thank you very much!

  5. #55

    Re: First steps for Super Mega Microbot

    Do you find a big difference between the "Onyx" black nylon versus Shapeways "Strong Flexible" in black? They're both nylon ...

    Also, for SMMB I might be able to make some parts in aluminum for cost of materials + tooling, as long as they can be done in 2.5D + flipping and rush speed wasn't important. Send me an email if there's something particular that would be useful for.

  6. Re: First steps for Super Mega Microbot

    Quote Originally Posted by jwatte View Post
    Do you find a big difference between the "Onyx" black nylon versus Shapeways "Strong Flexible" in black? They're both nylon ...
    They claim it is significantly stronger and stiffer than straight nylon. https://support.markforged.com/hc/en...209934486-Onyx

    Subjectively they certainly feel much stiffer than what I would expected from a normal strong and flexible print.

    Guess I should get those parts done at Shapeways too and compare.

  7. Re: First steps for Super Mega Microbot

    Continued progress, maybe slower than I'd like, but progress none the less...


  8. #58

    Re: First steps for Super Mega Microbot

    That is freakin' scary!

  9. #59
    Join Date
    Jun 2013
    Location
    Tucson, AZ
    Posts
    197
    Rep Power
    23

    Re: First steps for Super Mega Microbot

    Jump Jets!

Thread Information

Users Browsing this Thread

There are currently 2 users browsing this thread. (0 members and 2 guests)

Similar Threads

  1. Project The Stag - first autonomous steps
    By timmy_toner in forum Humanoids, Walkers & Crawlers
    Replies: 7
    Last Post: 04-13-2013, 06:19 PM
  2. Question(s) Up and walking with NUKE, next steps?
    By Lupulus in forum Software and Programming
    Replies: 13
    Last Post: 04-04-2013, 11:11 PM
  3. Project paid for laser range finder schematics and all steps
    By artifice in forum Projects For Request and/or Sale
    Replies: 1
    Last Post: 06-25-2011, 04:02 PM
  4. baby steps with the pololu servo controller
    By csdude in forum Arbotix, Microcontrollers, Arduino
    Replies: 25
    Last Post: 01-19-2010, 02:42 PM
  5. Super new to Bioloid need help please
    By sniperscope in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 02-25-2009, 07:55 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •