Page 3 of 6 FirstFirst 123456 LastLast
Results 21 to 30 of 59

Thread: First steps for Super Mega Microbot

  1. Re: First steps for Super Mega Microbot

    Fortunately, the rubber feet I've been using seem to work pretty well even as the angle changes during a contact sweep even with pretty steep contact angles. Two well publicized, but larger robots, (BD's Spot and MIT's Cheetah), use the same 3dof geometry, albeit with much more performant actuators.

    Stag, mentioned somewhere here in the forums, used a 4dof leg, with the 4th degree in the hip providing yaw control for each leg. It wasn't clear to me exactly what the benefit of adding that degree of freedom was if you had a foot which made contact at effectively one point, as Stag did.

  2. Re: First steps for Super Mega Microbot

    More slow but steady progress...

    The odroid shield came in from Macrofab, as did the mounting plates, servos, and feet supplies. I haven't brought up the daughterboard yet or wired everything, but did attempt a test mounting of everything but the turret today.

    Click image for larger version. 

Name:	IMG_5232.jpg 
Views:	121 
Size:	93.5 KB 
ID:	6130

  3. #23

    Re: First steps for Super Mega Microbot

    I think yaw would allow you to clear the legs from each other (and the body) when taking long strides.

  4. Re: First steps for Super Mega Microbot

    Now we've got things wired up, and have the our full software system running onboard:

    Click image for larger version. 

Name:	IMG_2315.jpg 
Views:	112 
Size:	109.6 KB 
ID:	6161
    Click image for larger version. 

Name:	IMG_2316.jpg 
Views:	116 
Size:	150.2 KB 
ID:	6162



    The gait engine is running at the 11.2ms HerkuleX frame interval, with IMU data currently being logged at 200Hz.

    Click image for larger version. 

Name:	2015-09-13-101959_1040x784_scrot.jpg 
Views:	108 
Size:	86.6 KB 
ID:	6163

    And we've moved our source repository to a public one at github, which includes all the software for the mech, the gait analysis tools, as well as the diagnostic tools like the plotting and telemetry manipulation:

    https://github.com/mjbots/mjmech

    Next up will be integrating the new turret with gimbal stabilization, then back to making it walk faster.

  5. #25

    Re: First steps for Super Mega Microbot

    OK, that looks cute!

  6. #26
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    30

    Re: First steps for Super Mega Microbot

    I like it! and can't wait to see more.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  7. #27
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    789
    Images
    276
    Rep Power
    76

    Re: First steps for Super Mega Microbot

    Hi. Great progress! Have you considered designing the body using vertical plates instead?
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  8. Re: First steps for Super Mega Microbot

    Quote Originally Posted by Zenta View Post
    Hi. Great progress! Have you considered designing the body using vertical plates instead?
    Thanks!

    So far I've only thought about vertical plates for the lizard configuration, where the HerkuleX mounting geometry doesn't make a single flat plate very convenient (as evidenced by the first iteration of this mech). For this configuration, I don't see a lot of downsides to the dual plate style: Manufacturing is trivial, it leaves lots of room to mount extra boards as necessary, and assembly and disassembly is really easy too. As shown here, I don't even have to mount the bottom plate unless I want a convenient place for a battery, or need to support the full weight of a mech warfare turret.

    What are your ideas for how vertical body plates would be useful?

  9. Re: First steps for Super Mega Microbot

    And now, finally, I have a working inertially stabilized gimbal! Neither it, nor the walking gait are necessarily tuned that well, but here's my youtube existence proof before I return to getting ready for Robogames!


  10. #30

    Re: First steps for Super Mega Microbot

    Walking and shooting. Scary!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Project The Stag - first autonomous steps
    By timmy_toner in forum Humanoids, Walkers & Crawlers
    Replies: 7
    Last Post: 04-13-2013, 06:19 PM
  2. Question(s) Up and walking with NUKE, next steps?
    By Lupulus in forum Software and Programming
    Replies: 13
    Last Post: 04-04-2013, 11:11 PM
  3. Project paid for laser range finder schematics and all steps
    By artifice in forum Projects For Request and/or Sale
    Replies: 1
    Last Post: 06-25-2011, 04:02 PM
  4. baby steps with the pololu servo controller
    By csdude in forum Arbotix, Microcontrollers, Arduino
    Replies: 25
    Last Post: 01-19-2010, 02:42 PM
  5. Super new to Bioloid need help please
    By sniperscope in forum Humanoids, Walkers & Crawlers
    Replies: 1
    Last Post: 02-25-2009, 07:55 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •