Hey,
Wandering through my local home improvement store I found some adhesive aluminum tape. I got some to test some fun hacking, like making electrodes for a touch-sensitive art installation, but instead ended up trying my hand at a low cost target panel design.
I have started preparing a little Mech-Warfare-style animation for next year, on a very low budget. The idea is to test the waters here in France before making any investment.
At first I thought we would use the japanese "Survival Game" type of hit sensor (with the aluminum foil cube) but then the previous paragraph happened, and now I have something that might make an electronic hit sensor feasible on our budget.
Having cheap target panels has been a question for some time around here (the previous complete set at $300 was a little bit pricey ), and some around here have provided some very interesting solutions, but I aimed at a little different set of constraints
- very cheap
- can be built with stuff from regular stores everyone has around (no custom PCB)
- fast and easy to build
- doesn't have to work perfectly on any mounting option, as I design these too and will make sure they are adapted.
So here it is :
Material for one full size panel :
- MDF 3mm : 2 squares of 76mm (=3 inches)
- Adhesive Aluminum tape 50mm wide: 150 mm
- 1.5mm outer diameter plastic tube : 80 mm
- double sided tape 50mm wide : 30mm
- regular sticky tape : around 500 mm
- some kind of spacing material (I used polar fleece 3mm thick : 60 x 30 mm )
Add to that some smallish silicone-insulated mutli-strand wire (I've used 24AWG), silicone wire is always so much more flexible.
* One of the square has a notch to get the cables out more easily, but with thinner wire or thicker spacer material (polar fleece) it could be avoided.
* The tube can be replaced with anything the right width and with a similar general morphology. Some hard cardboard, some wire, a toothpick, whatever as long as it serves the purpose explained below.
* The spacing material (polar fleece here) needs to be both compressible and very springy (some adhesive insulation foam, foam double sided tape, many types of synthetic fabric... ). The width of the tube thingy has to be adapted to the material used, so that it is maybe 0.5 to 1.5 mm thinner than the spacing material uncompressed, yet still thicker than the spacing material when it is compressed by the force of a BB hitting.
* I had MDF lying around but anything rigid, light-ish, that will resist to BBs without permanently deforming should work (plywood, PP...)
Assembly:
- Cut the tube into two parts smaller than the width of the aluminum tape
- Stick the aluminum tape flat on the square without the notch, and over the tubes on the other. The tubes have to be as close as possible to the edge but still fully trapped by the tape. Smooth the tape.
- strip the wires on 2 cm and fray them. Stick them on the aluminum, facing the notch (see picture below). The one on the square without the notch will have to go through the notch too when the assembly is finished, so make sure it's properly lined up.
- cut two 60x15mm rectangles of the spacing material (or other sizes depending on the material used, thinner for less compressible materials...) and tape them next to the tube thingy with double sided tape (see picture below).
- close the panel, and put tape around it (see picture below). Using a spacer between the plates to lock everything in place with the flat plate around 0.5 to 1mm above the tube thingy make it easier to get an acceptable assembly.
Tape does not adhere well to the rough side of the MDF stock I had, but it does to itself => simply make more than a turn, it is only there to keep the plates pressed against the spacing material.
- Done.
Many combination of materials could be used and the details of the assembly would have to be adapted.
I've made a few tests with this thing and so far it works well. Detection is good everywhere on the plate (a little harder in the center but I adjusted the spacing material to have it work nicely).
False hit detection when triggering a gun are entirely possible if mounted rigidly on the body of a bot that has the gun also mounted rigidly (witch seems like a bad idea to me anyway... mine will be mounted through shock absorbers). I'll try with various materials and mounting option. I'll try to lower the inertia of the hit plate, adjust the sensibility of detection, reduce transmission of the noise from the body to the plate.
The total cost of materials and assembly time, with a little refinement of the process, should be a few dollars a piece (mostly for assembly). They can nearly be considered disposable.
Not sure how they will compare to the original, since after all this time I still haven't been able to get official ones.
For now they will most probably be perfect for my low-cost version of the game though.
Bookmarks