I was reading some posts and came across a few on different weapons that people had posed or suggested and found it interesting. Most people seem to only want to compete in the air soft league, sadly all the creativity that people seem to have governing weapons design is stifled by their desire to only compete in this division. If reasonable safety precautions were taken to ensure the absolute security of these alternative weapons wouldn't it be feasible that these weapons be allowed in competition and not only allowed in hardcore class? Being that there is no mech warfare competition this year it would seem and there seems to be a lack of location for the competition as a whole , wouldn't a revision of the current rules be a help towards creating an improved event that would appeal to a larger audience so as to improve the hobby as a whole? This is just a thought there's no need to comment really. I just thought that a DC pump could safely fire bb's at another robot and that son people are more adept at making weapons than they are at making robots.
Bookmarks