Results 1 to 2 of 2

Thread: CM710 Embedded C with AtmetStudio6.2

  1. #1
    Join Date
    Jun 2013
    Location
    NW Arkansas
    Posts
    7
    Rep Power
    21

    Question CM710 Embedded C with AtmetStudio6.2

    Beside using the Boot Loader in RoboPlus Terminal, anyone found a way to connect direct their AVR/JTGICE/STK to CM710?

    Seems like the CM710 Chip is Atmega2561 where pin 11,12,13 looks like ICSP SCK, MOSI, MISO and they are hooked to 5 pin J1. Can't really tell which among the 5 pins is MOSI, RESET, SCK, MISO.

    Well, finding it would allow me to do live debugging using Atmel Studio on CM-710 board. Any help is appreciated.

  2. #2
    Join Date
    Jun 2013
    Location
    NW Arkansas
    Posts
    7
    Rep Power
    21

    Re: CM710 Embedded C with AtmetStudio6.2

    Might have got this one figured out by using a multitester and reading
    http://www.avrfreaks.net/index.php?n...=36477&start=0

    J1.Pin1=SCK same as J2.Pin9 SCK (PB1)
    J1.Pin2=MOSI same as J2.Pin3 CPU_RXD (PE0)
    J1.Pin3=MISO same as J2.Pin5 CPU_TXD (PE1)
    J1.Pin4=RESET same as J2.Pin6 Reset
    J1.Pin5=GND same as J2.Pin24 GND

    Only thing left is to solder a JST 5 pin with 1mm pitch.
    Last edited by Jim Cheong; 06-22-2014 at 11:49 AM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Bioloid Premium Kit with embedded C
    By Buell24 in forum Humanoids, Walkers & Crawlers
    Replies: 13
    Last Post: 06-02-2010, 12:50 PM
  2. Question(s) Learning embedded
    By Resilient in forum Robot Computers
    Replies: 6
    Last Post: 12-18-2008, 02:03 PM
  3. Discussion Embedded Newswire
    By LinuxGuy in forum Robot Computers
    Replies: 15
    Last Post: 12-02-2008, 01:22 PM
  4. Connecting Phidget Interface Kit to SBC with Windows Embedded
    By maennj in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 03-26-2007, 12:54 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •