Results 1 to 2 of 2

Thread: What happen with my 3.2" TFT???

  1. #1
    Percy L. Guest

    What happen with my 3.2" TFT???

    I got a problem with the 3.2" TFT. I connect the TFT module with Arduino MEGA 2560. Then I followed the instruction from http://forum.arduino.cc/index.php?topic=101029.0, downloaded UTFT library, used UTFT_demo 320x240 and changed the display model to SSD1289. It can show the demo, but with many thin white lines. The lines moves when the image moves.



    I have checked the wiring and it still happens. Any one knows why is that? Thanks for the help.

  2. #2
    Join Date
    Jul 2012
    Location
    Richmond, IN
    Posts
    652
    Rep Power
    38

    Re: What happen with my 3.2" TFT???

    Depending on how it is driving the lcd, the mega may be stuttering in it's output to the lcd, which expects it's input to be there at a certain timing which can change how the screen shows the image. (Many screens will also use this to adjust height and width of the picture on the screen itself)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Replies: 14
    Last Post: 06-27-2013, 07:38 PM
  2. Project "Free" "LIDAR"
    By Adrenalynn in forum Sensors
    Replies: 80
    Last Post: 11-16-2012, 12:27 PM
  3. Project Bioloid 6x6 rocker-bogie suspension little "Mars curiosity"
    By siempre.aprendiendo in forum Rovers
    Replies: 2
    Last Post: 12-12-2011, 01:38 PM
  4. Bioloid RoboPlus - "A file motion cannot play Next/Exit pages....."
    By aacs in forum Humanoids, Walkers & Crawlers
    Replies: 5
    Last Post: 09-22-2011, 03:27 AM
  5. Replies: 1
    Last Post: 05-15-2009, 01:57 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •