Results 1 to 2 of 2

Thread: Battery recommendation for mx-64t dynamixels

  1. #1
    adityassripada Guest

    Battery recommendation for mx-64t dynamixels

    We are using a set of 6 MX64-T Dynamixels connected in a daisy chain for a biped.Which batteries will be ideal to power up these Dynamixels ? Each of the Dynamixel draws 4.1A at 12V.

    Can we connect the batteries directly to the Open CM 9.04's battery slots directly to power-up the motors ?

    Controller : Open CM-904B

    Motors : MX-64T Dynamixels

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    284

    Re: Battery recommendation for mx-64t dynamixels

    The MX-series servos work best with 12V (3S LiPo). The battery should be labeled with a 'C' rating that, combined with the capacity, will tell you how much current the battery can safely provide to the servos (2300mAh capacity * 15C_continuous_rating = 34.5A continuous). The 'recommended' torque is ~1/5 of the stall torque and the MX-64T should only require 4.1A when stalled, so the sustained current of all the servos should be a bit less than 6*4.1A but failing to meet the surge current requirements can cause serious issues (servos can behave erratically and sometimes reset their IDs).

    The pair of series wired, two-pin battery connectors on the OpenCM-904 are only rated ~2A, and intended primarily for XL-320 servos with the pair of 1S LiPo batteries of the Darwin-Mini (AX-12 are usable when powered through the CM-904 with 3S LiPo, but it is still best to add a powered hub). You will need to power the MX-64T servos through something like the trossen AX/MX powered hub or custom cables to connect the battery to the power and ground pins of the servos.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. New low-cost Dynamixels and a controller!
    By guruguhan in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 01-04-2014, 03:26 PM
  2. Question(s) how many dynamixels can an arduino handle?
    By vassilissa in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 10-25-2013, 01:26 PM
  3. Question(s) Recommendation on beginner controller?
    By TResell in forum Robotics General Discussion
    Replies: 5
    Last Post: 03-22-2013, 05:45 PM
  4. Off-Topic: Webcam recommendation request
    By Stobs in forum Mech Warfare
    Replies: 4
    Last Post: 09-10-2010, 11:14 PM
  5. Question(s) Need recommendation for USB or PCMCIA to RS232 (For AVR or PIC use)
    By nizee in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 03-25-2010, 11:50 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •