Results 1 to 3 of 3

Thread: MX-64- which model of Maxon motors?

  1. #1

    MX-64- which model of Maxon motors?

    Does anyone know which Maxon motor is used for MX-64? There is some number on the motor but could find it in the online catalog

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    278

    Re: MX-64- which model of Maxon motors?

    If you have damaged the motor, get an RMA and have Robotis fix it. Because Robotis has the pinions welded onto the motors by Maxon, all the motors in their servos get custom model numbers. You can probably get the general model by matching as much of the model number as you can, but you will not find the exact model in their catalog.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. #3

    Re: MX-64- which model of Maxon motors?

    thanks for the reply tician!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Dynamixel MX-28T: installed Maxon RE-max motor?
    By fjp in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 05-30-2013, 07:12 AM
  2. 3D Model Thread?
    By YoMarchYo in forum Mech Warfare
    Replies: 0
    Last Post: 04-07-2013, 02:40 AM
  3. 0.2" FSR integration with MAXON EPOS2 P
    By mihir in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 05-08-2012, 08:31 AM
  4. Replies: 0
    Last Post: 05-06-2012, 09:23 PM
  5. CAD Model of Phidgets
    By cmmguy in forum Arbotix, Microcontrollers, Arduino
    Replies: 9
    Last Post: 04-23-2008, 03:56 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •