Results 1 to 2 of 2

Thread: Caster wheels and offset?

  1. #1
    tysonmarconi Guest

    Caster wheels and offset?

    I was wondering why many casters I see have a horizontal offset that, at minimum is equal to the radius of the wheel. I understand that the amount of force required to turn the wheel will go up, and the pivot velocity will increase. Is there a fundamental reason why many mass manufacturers choose to go with larger offsets? I'd like to minimize the offset due to space constraints.

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,282
    Images
    27
    Rep Power
    275

    Re: Caster wheels and offset?

    Basic answer is that if you do not offset the center of the wheel from the center of caster rotation (if the two axes of rotation intersect), the wheel will simply skid sideways instead of changing direction of travel when moving forward then pushed sideways. The larger the offset, the easier it is for the wheel to turn to the direction the caster mount is being moved but it also increases the torque on the caster bearing (increases cost) and increases in-place skidding/swerving of the the wheel (increases tread wear) during low speed maneuvering and/or rapid/complete direction changes.

    There are ball casters in smaller sizes, omni-wheels can work in some larger situations, and you can make your own ball caster using 3+ omni-wheels equally spaced on top a large sphere.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Wheels for Dynamixel Servos
    By SamQ in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 07-27-2011, 07:56 PM
  2. Replies: 4
    Last Post: 12-17-2010, 09:42 AM
  3. Banebots, wheels, batteries
    By idkruler in forum Garage Sale
    Replies: 0
    Last Post: 08-03-2009, 11:42 PM
  4. I need help with the bioloid humanoid offset
    By flS97 in forum Humanoids, Walkers & Crawlers
    Replies: 3
    Last Post: 03-03-2009, 05:59 PM
  5. Colson Wheels to 6mm Shaft
    By Judge in forum Mechanics / Construction
    Replies: 4
    Last Post: 06-06-2008, 08:38 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •