Results 1 to 1 of 1

Thread: Robotis Task

  1. Robotis Task

    working on a balance page for my robot and so far got the gyro to turn off and on, also can control any joint with the gyro while it is on --MOTION INDEX 3-- Also have activated the --SLIP-- so that if it falls forward or backward the slip changes accordingly and shuts off my --AUX LED-- like it is supposed to


    --MOTION INDEX 3-- is a repeating page

    the problem is I cant get the robot to change motions and the program just freezes
    Attached Thumbnails Attached Thumbnails Click image for larger version. 

Name:	image.jpg 
Views:	210 
Size:	103.9 KB 
ID:	5686   Click image for larger version. 

Name:	image.jpg 
Views:	200 
Size:	102.2 KB 
ID:	5687  

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. need help Cm-510 roboplus task code
    By Ron in forum Software and Programming
    Replies: 2
    Last Post: 11-05-2012, 10:06 PM
  2. Question(s) On Bioloid: How did Robotis make the CALLBACK function in RoboPlus Task?
    By cybernetics in forum Software and Programming
    Replies: 6
    Last Post: 09-11-2011, 03:09 PM
  3. Question(s) Using CM-5 with Roboplus Task
    By jarred in forum Software and Programming
    Replies: 4
    Last Post: 04-30-2010, 12:04 PM
  4. Robot Task Planning Approaches?
    By Pi Robot in forum Robotics General Discussion
    Replies: 4
    Last Post: 04-29-2010, 12:37 PM
  5. Question(s) Writing a task scheduler
    By badcommandorfilename in forum Software and Programming
    Replies: 12
    Last Post: 03-14-2010, 09:17 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •