Results 1 to 3 of 3

Thread: Problem with PhantomX powersupply

  1. Question Problem with PhantomX powersupply

    Hi,

    I recently purchased the PhantomX hexapod, assembled it according to the online manual and charged the battery with the delivered charger.

    I can connect the robot to the PC and the "Blink" Demo code is uploadable and working.

    When I try to run the "Hexapodtest" - Code, the Serial monitor gives the following message:

    ###########################
    Serial Communication Established.
    ###########################
    System Voltage: -0.10 volts.
    Voltage levels below 10v, please charge battery.

    This is rather strange, since the battery should be at about 11.5-12V according to the charger and the little monitor included in the kit.

    I attempted to skip the "checkvoltage" command, the servos were actually moving, but not in the right way.


    I wired everything according to the manual and the circuit seems fine when I look at it.

    Arbotix-M is set to VIN, connected to the Power Hub in the back which is supplied by the battery.
    2 legs are connected to the arduino board and 4 to the power hub, their IDs should be preset in this model.


    Does anybody have a suggestion what could be wrong? I`d appreciate any kind of help,

    greetings L

  2. #2

    Re: Problem with PhantomX powersupply

    There's actually a bug in the test code - the voltage check command looks for the servo ID # 1 to report the voltage - so if there's not servo #1, the system mistakenly says 'low voltage' instead of 'servo missing'

    I'm guessing that either a)you are missing servo 1 or more likely b)at least 2 servos have ID # 1.

    When you commend out 'CheckVoltage' what data did you get from the serial monitor?

    Did you go through the ID guide?
    http://learn.trossenrobotics.com/ind...tool#&panel1-1

  3. Re: Problem with PhantomX powersupply

    You are absolutely right, I actually found a similar thread in the forum after I posted this, I couldn`t delete mine in time though.

    After I changed the IDs of the Servos it worked properly, thank you.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) AX-12A Control Problem(function dxl_write_word problem)
    By sorcun in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 06-14-2013, 12:04 PM
  2. Question(s) PhantomX AX Quadruped Mark II PhantomX Robot Turret Equipped??
    By hwan we in forum Robotics General Discussion
    Replies: 1
    Last Post: 03-11-2013, 03:09 PM
  3. ROS problem -> cv_bridge: problem transfering images between nodes
    By Median in forum ROS - Robot Operating System
    Replies: 0
    Last Post: 03-11-2013, 10:44 AM
  4. For learning: PhantomX Hexapod vs PhantomX Quadruped
    By Leugim in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-26-2012, 09:50 AM
  5. One problem after another!
    By bidi in forum Arbotix, Microcontrollers, Arduino
    Replies: 22
    Last Post: 02-02-2007, 03:39 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •