Results 1 to 5 of 5

Thread: Experiment with linear actuators

  1. Experiment with linear actuators

    I was looking to build a robot arm with a reasonable lifting capacity (couple of kilos), and had difficulty finding something stronger than robot servos but cheaper than a full-spec industrial arm. The solution I have come up with is to use linear actuators for the main lifting components, and I think I will probably use Dynamixels for the wrist/gripper.
    Here is a video of in action (sorry about the lighting):

    I think this approach is pretty promising.

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    285

    Re: Experiment with linear actuators

    Linear actuators are great when you don't have to worry about humans. They are strong, precise, and fairly inexpensive (to buy or build), but slow and non-backdrivable (definitely electric lead screw versions; pneumatic and hydraulic can be a bit more forgiving under some conditions). This means that if anything gets in their way, then they will keep going until they destroy their internal drive system, the structure to which they are attached, and/or anything in their way. Of course, the very expensive Dynamixel Pro servos use a non-backdrivable cycloidal drive, so should be fine as long as you include plenty of protection against contact with foreign objects (padding and/or FSR skin for contact sensing).
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. Re: Experiment with linear actuators

    Good points - the laws of robotics suggests that I should not try to harm anyone. I saw somewhere that someone had added a stiff spring with displacement measurement to a linear actuator to create compliance and force measurement for both safety and control.
    This also seems like an interesting idea.

  4. #4
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    285

    Re: Experiment with linear actuators

    You could also use springs and cables to transmit the forces with compliance while keeping the linear actuators safely tucked inside a housing. The DLR hand uses dyneema fibers, motorized capstans (position control), and motorized roller-arms (real-time adjustable cable tensioners and torque sensors) to make a very fancy and durable arm/hand - they can hit the fingers with a hammer, then put the hammer in the hand to drive nails. The 'low-cost compliant 7-dof robotic manipulator' from a group at Stanford (circa 2011) uses stepper motors for the big timing-belt/cable-driven joints in the shoulder and elbow then uses dynamixels for the hand and wrist.

    I bought two spools (500m black and 300m blue) of generic 100lbf dyneema multi-strand fishing line for ~$25 to experiment with a cable-driven arm but still have not gotten around to using it for robots. Have to be careful with the stuff; it is so thin and strong that it can rather easily cut through flesh and itself when tensioned.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  5. Re: Experiment with linear actuators

    Here's a little update to the design using the position feedback to allow control via USB.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Discussion Making your own Linear Actuators
    By stilgarhammer in forum DYNAMIXEL & Robot Actuators
    Replies: 5
    Last Post: 11-17-2012, 10:30 PM
  2. Linear actuators and springs for walking?
    By randy921 in forum Humanoids, Walkers & Crawlers
    Replies: 8
    Last Post: 07-10-2012, 11:22 PM
  3. Question(s) Mini Style 4" Stroke 8lbs Force Linear Actuators 12v
    By InfoSponge in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 04-28-2011, 11:57 PM
  4. Question(s) How to control 3 linear actuators by computer?
    By Leaw in forum DYNAMIXEL & Robot Actuators
    Replies: 7
    Last Post: 06-03-2010, 11:16 PM
  5. SSC-32 Controllable linear actuators?
    By Rift in forum DYNAMIXEL & Robot Actuators
    Replies: 40
    Last Post: 04-11-2009, 08:03 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •