Results 1 to 7 of 7

Thread: Mark I phantom Hexapod

  1. Mark I phantom Hexapod

    I have been trying to upload the Phantom x AX-12 stock code onto my Mark I hexapod, using an FTDi as the programmer. When it gets to the uploading part LED will Flash on the Arbotix board then turn off after 2-3 seconds. I tried pressing and holding the reset button on the board as well. The code will sometimes upload but it isn't consistent.

  2. #2

    Re: Mark I phantom Hexapod

    Do you get any errors in the Arduino IDE?

    Are you suing the Original ArbotiX or the ArbotiX-M?

  3. Re: Mark I phantom Hexapod

    Quote Originally Posted by kgranat View Post
    Do you get any errors in the Arduino IDE?

    Are you suing the Original ArbotiX or the ArbotiX-M?

    Yeah, It was the avrdude not in sync sk000 error, and I believe it is just the Arbotix

  4. Re: Mark I phantom Hexapod

    Yeah it is the avrdude not in sync sk000 0x00 error and I am using the arbotix

  5. Re: Mark I phantom Hexapod

    Yeah, I get the error avrdude not in sync sk000 0x00 and I am using the arbotix.

  6. #6

    Re: Mark I phantom Hexapod

    Do you have anything else plugged into the board when your programming? You can't have your XBee plugged in while programming over FTDI.

    Do you have access to an ISP programer? You might try to reload the bootloader.

    If all else fails, let me know and you can send the board back and we'll either fix or replace it.

  7. Re: Mark I phantom Hexapod

    I didnt have anything plugged into the board besides the FTDI, I am going to try to upload the code via the two paired xbees. If that doesn't work then I will try to flash the bootloader on the board

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Next steps with a PhantomX AX Hexapod Mark II & BBB
    By CreedyNZ in forum Software and Programming
    Replies: 62
    Last Post: 08-23-2016, 06:46 AM
  2. News/Announcement PhantomX AX Hexapod Mark II Kit
    By etwx in forum Garage Sale
    Replies: 2
    Last Post: 04-08-2014, 08:31 PM
  3. Problems in power uo the phantom hexapod mark ii kit
    By robot$ in forum Humanoids, Walkers & Crawlers
    Replies: 33
    Last Post: 07-19-2013, 02:48 AM
  4. Phantom X Mark II new tibia design?
    By TXBDan in forum Humanoids, Walkers & Crawlers
    Replies: 10
    Last Post: 06-21-2013, 08:13 AM
  5. Phantom X Mark II AX-18A Hexapod - Approx runtime on supplied LiPo?
    By Grumpybeard in forum Humanoids, Walkers & Crawlers
    Replies: 3
    Last Post: 04-12-2013, 01:42 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •