Results 1 to 2 of 2

Thread: RX24 need help with getting position with Arduino Mega

  1. Honorablemention RX24 need help with getting position with Arduino Mega

    Hi guys, I bought RX24-f servo but I could not get the position feedback from that servo, actually I have used cheaper servos before but
    I'm newbie for RX24-f. I have no money for control board CM700, could you please lead me a way to get the position feedback from it by using arduino mega and MAX 485 circuitry. I constructed the arduino mega and MAX 485 circuitry than I turned on/off the led however could not find anything for getting position feedback from it. I watched many videos, and all of them using CM 700 etc. Could you help me please?

  2. #2

    Re: RX24 need help with getting position with Arduino Mega

    Robotis manuals are here: http://support.robotis.com/en/
    RX-24F is here: http://support.robotis.com/en/produc...ies/rx-24f.htm

    Information about the protocol can be found here: http://support.robotis.com/en/produc...munication.htm
    To get position feedback, read registers 36/37 (Present Position) Note that it's a two-byte value that has to be concatenated to a 16-bit integer.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Dynamixel Servo Control Issues (MX-28 and Arduino Mega)
    By JasonT in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 08-12-2014, 08:12 PM
  2. Arduino Mega 2560 and Serial Comunication issues
    By DVS in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 07-10-2013, 03:31 PM
  3. Arduino Mega 2560 and AX12A servos
    By DVS in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 07-08-2013, 05:26 PM
  4. Arduino Mega 2560 and AX12A servos
    By DVS in forum Sensors
    Replies: 1
    Last Post: 07-08-2013, 05:09 PM
  5. Question(s) controlling 6 ax-12a's with an arduino Mega
    By mlerner in forum DYNAMIXEL & Robot Actuators
    Replies: 6
    Last Post: 02-01-2013, 06:29 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •