Results 1 to 4 of 4

Thread: Double Eagle gearbox questions

  1. #1

    Double Eagle gearbox questions

    I've had some failures by the double eagle gearboxes recently, and wanted to compare notes.

    First, one gearbox seems to have stripped itself (or otherwise lost its gear meshing) such that the gear trying to pull back the action just shakes, and some gear further up the gearbox chain keeps slipping (with a nasty sound.) I've tried inspecting the gears through the plastic, but it's kind-of fuzzy, and there's some lubricant gunk in the way, and I can't see anything obviously broken. Yet, it doesn't work. Has anyone else seen this, or is it uncommon?

    Second, when battery powered (11.1V LiPo, charged, about 11.4V) the gearbox motors fail to actually pull the action completely and stall, using a 50%-60% PWM duty cycle. Meanwhile, when using a 11V/5A power supply (that drops voltage for over-current) and the same duty cycle it works fine. It also works fine when using 6V voltage and no PWM. The power supply and the battery join at the same power entry plug, so there's no difference in wiring (actually, the power supply has longer/thinner wires to that point.) The battery is rated 20C and can run fourteen MX-64 servos just fine.
    The failure acts like a stall of the motor -- nothing turns. Touching 6V +/- straight to the motor will make it turn past the stalling point.
    What am I missing here; why is the battery different from the power supply?

  2. #2

    Re: Double Eagle gearbox questions

    The second question has an answer: I have wired my feed/un-jammer to switch 1, and fire to switch 2, on the Onyx Fire board.
    However, I wrote the registers to set the duty cycle to 25% on switch 2, and 50% on switch 1, reverse from what I intended.
    An oscilloscope quickly showed me what the problem was; I should have hooked it up earlier :-)

    First question is still outstanding: How durable are these gear boxes, really?

  3. #3
    Join Date
    May 2010
    Location
    Princeton University
    Posts
    354
    Rep Power
    39

    Re: Double Eagle gearbox questions

    Quote Originally Posted by jwatte View Post
    First question is still outstanding: How durable are these gear boxes, really?
    From what I have seen, not very. I have broken them just by running them too fast (11v). I remember stripping a gear on 1 or 2 of them doing that.

  4. #4

    Re: Double Eagle gearbox questions

    Thanks! At least that validates my experience :-)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. gearbox 3d model
    By sthmck in forum Mech Warfare
    Replies: 1
    Last Post: 12-11-2014, 08:54 PM
  2. RC Servo Gearbox Questions
    By byi in forum Mech Warfare
    Replies: 18
    Last Post: 01-08-2014, 11:24 AM
  3. AX-18F = AX-12+ with a double torque. Crazy idea?
    By RobotAtlas in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 06-13-2010, 07:34 PM
  4. Question(s) motor/gearbox for heavy lawnmower-rover?
    By wrongprotocol in forum Rovers
    Replies: 12
    Last Post: 04-29-2009, 10:36 AM
  5. produce gearbox,toy tyre,motor driver
    By gzresident in forum Projects For Request and/or Sale
    Replies: 0
    Last Post: 03-01-2009, 09:00 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •