Results 1 to 3 of 3

Thread: Hokuyo UTM 30-LX measurement problems

  1. Hokuyo UTM 30-LX measurement problems

    Hi everyone,

    I'm working with hokuyo UTM 30-LX on my project. This sensor has 0.1 to 30 meters range. However sometimes it gives me 1 millimeter as distance measurement. But when an object is putted in that spot it measures correctly. Approximately %10 of my measurement consist of this wrongly measured 1 millimeter. What could be reason of this problem?
    Attached Thumbnails Attached Thumbnails Click image for larger version. 

Name:	Ekran Resmi 2014-12-26 13.18.41.jpg 
Views:	267 
Size:	64.0 KB 
ID:	5741   Click image for larger version. 

Name:	Ekran Resmi 2014-12-26 13.19.13.jpg 
Views:	249 
Size:	64.9 KB 
ID:	5742   Click image for larger version. 

Name:	Ekran Resmi 2014-12-26 13.19.24.jpg 
Views:	263 
Size:	51.5 KB 
ID:	5743   Click image for larger version. 

Name:	Ekran Resmi 2014-12-26 13.19.35.jpg 
Views:	273 
Size:	54.8 KB 
ID:	5744  

  2. #2

    Re: Hokuyo UTM 30-LX measurement problems

    First: Lucky you; that's a nice piece of gear :-)

    Second, I don't have one, but when I've seen other ranging sensors report too-close data, it's been because of self-reflection.

    If you need to get this working right away, perhaps you can work around it by discarding any measurement less than, say, 10 mm, and interpolate between the surrounding measurements?
    Then, when the Hokuyo people come back from break, perhaps you can get in contact with an application engineer and ask them directly.

  3. #3
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,314
    Images
    27
    Rep Power
    279

    Re: Hokuyo UTM 30-LX measurement problems

    According to the URG Network tutorial under 'Range Data' and the first question of the FAQ, the device will return a value lower than the minimum distance whenever an object is not detected within its sensing range. Sensing range can be affected by angle of incidence, lighting intensity (UTM-30-LX spec sheet says it is intended for ~1000lx indoor lighting), object reflectance (dark objects reflect less light), and object width (minimum width increases with distance from sensor).
    Last edited by tician; 12-26-2014 at 01:44 PM.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Implementing Hokuyo URG-04LX to Hector_SLAM
    By kevin_05 in forum Sensors
    Replies: 0
    Last Post: 07-25-2014, 04:16 AM
  2. Need help for selecting sensors for deflection measurement
    By Preety in forum Robotics General Discussion
    Replies: 16
    Last Post: 07-10-2014, 11:52 AM
  3. Question(s) ROS Hydro, Hokuyo UR-04LX and BBB
    By kevin_05 in forum Sensors
    Replies: 12
    Last Post: 06-09-2014, 10:10 PM
  4. Question(s) motion and measurement models for Kinect
    By ajp in forum Sensors
    Replies: 1
    Last Post: 07-13-2013, 11:34 PM
  5. Question(s) Hokuyo laser Range finders
    By athukoralakasun in forum Sensors
    Replies: 6
    Last Post: 02-10-2013, 02:08 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •