Results 1 to 4 of 4

Thread: stationary Powering an Open CM 9.04-b with 3 Dynamixels

  1. stationary Powering an Open CM 9.04-b with 3 Dynamixels

    Hi There!


    I'm totaly new to Robotics and Microcontrollers and in my first project i want to build something similar as a Pan/Tilt/rotate Plattform. I'm thinking about using the Open CM 9.04-B which controlls 3 AX-12A's (or maybe 3 MX12W's)


    But how do i power it without using LiPo's ? i dont really want to start by cutting and soldering cables. SMPS2Dynamixel ? but then what is the power switch for ? And in this case - do i still need the microUSB to power the board ?




    Thanks!

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,315
    Images
    27
    Rep Power
    279

    Re: stationary Powering an Open CM 9.04-b with 3 Dynamixels

    The switch is for controlling power supplied by two 1S LiPo batteries connected to the two 2-pin JST-PH headers. If you want to control AX or MX servos with a 3S LiPo, you will need to connect the LiPo pack to either the 0.1" headers marked VIN+/VDD_IN and VIN- (which will be controlled by the switch), or connect the pack through a DXL hub or SMPS2Dynamixel. The traces on the OpenCM904 are not very heavy duty, so you will probably want to go with a DXL hub or SMPS2Dynamixel if you are planning to have the servos running at high load. If you supply any external power to the OpenCM904 of more than ~6V then you should not need to connect USB except for communications.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  3. Re: stationary Powering an Open CM 9.04-b with 3 Dynamixels

    ok, great!

    thanks for the answer!

  4. #4

    Re: stationary Powering an Open CM 9.04-b with 3 Dynamixels

    I agree with Tician -- power it through a hub. The hub will in turn power the OpenCM, so you only need the USB for communication.
    (FWIW, this is what I do on Onyx 7)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Replies: 4
    Last Post: 04-16-2014, 08:39 AM
  2. Question(s) Powering serializer wl 3.0
    By herzeleid in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 01-04-2011, 12:07 PM
  3. Powering a Roboard
    By mattmaho in forum Power
    Replies: 3
    Last Post: 05-03-2010, 06:02 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •