Page 2 of 2 FirstFirst 12
Results 11 to 12 of 12

Thread: Interfacing FLIR Lepton with Intel Edison

  1. Re: Interfacing FLIR Lepton with Intel Edison

    @jwatte
    I don't have any other components in my current setup beside the Edison as the I2C master, the level shifter in-between and the Lepton as the one and only I2C slave on the bus. My MCP9808 and ADXL345 sensors work as they should with this configuration. As you can see from the attached image the I2C SCL pin from the Edison should be ok (not yet toasted) when using a 1K Ohm pullup.


    Name:  Edison_Lepton_1V8_I2C_SCL_NOTHING.png
Views: 354
Size:  26.7 KB


    It must have something to do with the Lepton. What coul'd I do about a weak driver?
    Last edited by McRender; 03-04-2015 at 03:39 AM.

  2. Re: Interfacing FLIR Lepton with Intel Edison

    Quote Originally Posted by McRender View Post
    I don't have any other components in my current setup beside the Edison as the I2C master, the level shifter in-between and the Lepton as the one and only I2C slave on the bus.
    I lost lock on which combinations worked and didn't. Could you post the circuit diagrams for the Raspberry (i.e the LEPTON one that worked) and Edison (i.e. the sensor ones that worked and the latest LEPTON one that didn't)?

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Experiment with Intel Edison...
    By KurtEck in forum Arbotix, Microcontrollers, Arduino
    Replies: 99
    Last Post: 05-27-2015, 01:36 PM
  2. Intel NUC
    By CogswellCogs in forum Robot Computers
    Replies: 25
    Last Post: 11-09-2013, 06:04 PM
  3. interfacing SSC 32 with max msp
    By arduinooo in forum Software and Programming
    Replies: 3
    Last Post: 01-30-2013, 05:03 PM
  4. I-sobot + Arduino interfacing made easy
    By Nelsontheunholy in forum Humanoids, Walkers & Crawlers
    Replies: 0
    Last Post: 01-21-2010, 03:17 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •