Results 1 to 2 of 2

Thread: RG90 Gear Motor--where to find spur gear?

  1. #1
    Omegasamurai Guest

    Exclamation RG90 Gear Motor--where to find spur gear?

    Hey guys!

    I'm trying to get a gear I can put on the output shaft of this RG90 DC gear-motor that I need for a senior project type thing.
    Problem is, I can't find very much information about the gear motor at all; no data sheet or anything, and I can't find any spur gear that fits the output shaft size on this motor which is 3.5 mm in diameter.

    If any of you have used this motor and you know where to find any of this, It'd be greatly appreciated. Thanks.

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    279

    Re: RG90 Gear Motor--where to find spur gear?

    Do you mean the RG90 here, and its technical drawing with main electrical/mechanical specs (WHY?!?!? Torque is not 'kg/cm', it is 'kg-cm'; torque is equal to 'force times length', same units as energy)? Probably not since that one has a 7mm OD shaft with double flats (yet no measurement of the thickness across flats, or length of flats) intended for compatibility with solarbotics plastic gearmotors.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Where to find internal gear?
    By Harryk in forum Mechanics / Construction
    Replies: 2
    Last Post: 01-25-2013, 12:15 PM
  2. Servo gear lash
    By danhoskin in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 03-01-2010, 11:23 AM
  3. Question(s) Worm gear in Servo?
    By sam in forum DYNAMIXEL & Robot Actuators
    Replies: 32
    Last Post: 09-16-2009, 03:05 PM
  4. Recommends on DC gear-motor, that can output > 10ft/lbs
    By scowby in forum DYNAMIXEL & Robot Actuators
    Replies: 17
    Last Post: 08-03-2009, 12:33 PM
  5. correct Set Screw Hubs for AME-218 gear motor
    By scowby in forum Mechanics / Construction
    Replies: 3
    Last Post: 07-29-2009, 03:59 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •