Although as mentioned, having firmware specifically for ROS would simplify things of course.![]()
Although as mentioned, having firmware specifically for ROS would simplify things of course.![]()
For using a arobotix with ros I have a turtlebot2 with a custom done Turtlebot arm on top.(https://plus.google.com/+BlackStag/posts/hGfyr8PrmC1)
I have a large outdoor robot 6 wheel (Jrover) using vex pro controller and ros serial. (http://www.dfrobot.com/community/?p=4026)
I have a couple more custom base ones that use various arm boards for testing.
Did not know they were bothering to upgrade it, but all the relevant specs are on their product page. There are a few errors in the comparison table as the old fit-pc2i does have gigabit ethernet and the wifi is only limited to 802.11g by the crap drivers of the default ubuntu 10.04 install. The wifi module is fully capable of 802.11n after upgrading the OS. They don't say much about the CM-740, but it does not look like it actually 'improved' so much as simply rearranged to fit the new processor board as it appears to still use two inertial ICs instead of a cheap all-in-one sensor.
edit: if the above seems angry and/or annoyed, it is partly because we lost the third dehumidifier in ~8 years a couple days ago. How can it possibly be so damn difficult to make a dehumidifier that will not puke its refrigerant within 2~4 years of purchase? Had a 'dumb' dehumidifier that lasted somewhere around a decade before the bucket cracked and several more years before the control board finally crapped out. The Haier lasted little more than a year before it dumped its refrigerant. The first LG lasted less than 2 years before the humidity sensor crapped out and the control board would not run without it. The extended warranty replacement LG lasted maybe 3 years before it developed what I expect was a pinhole leak in a solder joint somewhere and continued limping along for a few months before it suffered a catastrophic rupture a couple days ago. Basement is still filled with the horrid stink of refrigerant ~3 days later and need to set up a fan and plastic sheeting to flush it out of the house; sorry earth.
Last edited by tician; 03-19-2015 at 01:15 AM.
Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
"You have failed me, Brain!"
[git][mech][hack]
gives free advice only on public threads
Because warranties are 1 year.How can it possibly be so damn difficult to make a dehumidifier that will not puke its refrigerant within 2~4 years of purchase?
Welcome to the American market, where everyone buys on purchase price alone and quality is a race to the bottom!
Had to search a bit, but the ROBOTIS-OP 2.0 mother board is an AAEON PICO-CV01 without the VGA connector.
Last edited by vehemens; 03-21-2015 at 10:11 PM.
Getting back to ROS, I did find some information on DARwIn-OP simulations using Gazebo and ROS a while back but haven't had a chance to try it myself.
Forgot to mention there's also NimbRo ROS for those with bipeds.
There are currently 1 users browsing this thread. (0 members and 1 guests)
Bookmarks