Page 3 of 3 FirstFirst 123
Results 21 to 25 of 25

Thread: How to choose battery for high torque motors?

  1. Re: How to choose battery for high torque motors?

    Quote Originally Posted by tician View Post
    Just never let the LiPo drop below 3.2V per cell or charge above 4.2V per cell.
    Thanks. May I ask how and why? I thought charger would charge at the appropriate voltage automatically.

  2. Re: How to choose battery for high torque motors?

    Thanks jwatte for the info.

  3. #23
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,285
    Images
    27
    Rep Power
    275

    Re: How to choose battery for high torque motors?

    If you buy a decent LiPo balancing charger, then you should have no problem charging. The cheap battery monitors/alarms mentioned earlier will help protect against over discharging.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    bleh

  4. #24

    Re: How to choose battery for high torque motors?

    May I ask how and why?
    If you use an appropriate charger, and use it correctly, then you are unlikely to have a problem with over-charging.
    The world is full of people who don't necessarily follow those suggestions at all times, though. And chargers that fail.

  5. Re: How to choose battery for high torque motors?

    Thanks

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. ~1RPM high torque motor or servo
    By timothyahong in forum DYNAMIXEL & Robot Actuators
    Replies: 0
    Last Post: 06-26-2011, 02:43 PM
  2. Question(s) Recommendations for high capacity Lithium ion battery packs?
    By Pi Robot in forum Power
    Replies: 12
    Last Post: 09-20-2010, 02:06 PM
  3. Question(s) How to choose the correct size motor controller
    By hiltoab in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 08-03-2010, 01:29 AM
  4. Project designing high torque motor
    By robot maker in forum Mechanics / Construction
    Replies: 15
    Last Post: 10-02-2008, 12:47 AM
  5. Which to choose to start???
    By LiTTle in forum Software and Programming
    Replies: 1
    Last Post: 07-24-2008, 12:27 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •