Results 1 to 3 of 3

Thread: Abotix Pros - Troubleshoot

  1. #1

    Abotix Pros - Troubleshoot

    Hi,

    what does it means if I dont see 4 solid green light on the arbotix pro controller, I never see them but everything seems to work fine anyway.

    I see only the two leds in the back steady green, but I see 2 transparent led that should be steady green according to the Video tutorial

    https://github.com/Interbotix/HROS1-...aspberry-Pi%29

    SHould I reset it? Is it bad?

  2. #2
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    141

    Re: Abotix Pros - Troubleshoot

    The two LEDs near the power jack are for power indication, those are the most important.

    The other pair of LEDs near the USB are for FTDI communication. Sometimes the FTDI will toggle these on/off randomly on startup, so disregard needing these to be lit up.

    The set of 3 LEDs near the buttons should flash rapidly 3 times when the Arbotix-Pro is first powered on, this indicates the firmware is booting up and launching the main code loop properly.

  3. #3

    Re: Abotix Pros - Troubleshoot

    OK YAAAY!! It means everything is okay, anyway except for servo #13, everything is fine with the robot.

    Best regards, we can close this topic then

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •