Page 3 of 8 FirstFirst 1234567 ... LastLast
Results 21 to 30 of 72

Thread: HR-OS1 3D Models & 3D Printed Armor

  1. #21

    Re: HR-OS1 3D Models & 3D Printed Armor

    Hi, say how does this shapeways store you were going to set up work? I have never shipped out for parts (3-D parts) so will this
    be like a package/kit that we can buy from you all or what? I'm working with different materials on my 3-D printer right now, seems all abs formulas are not the same.

  2. Re: HR-OS1 3D Models & 3D Printed Armor

    Hi All,

    I have just print the head

    Click image for larger version. 

Name:	WP_20150507_17_57_09_Pro.jpg 
Views:	189 
Size:	98.6 KB 
ID:	5915

  3. #23

    Re: HR-OS1 3D Models & 3D Printed Armor

    OMG! This dam 3-D printer is mesmerizing me.

  4. Re: HR-OS1 3D Models & 3D Printed Armor

    I had a question regarding the head: Why was this shape chosen over the other shape heads I've seen (like the "traditional" Jimmy head). Was it the weight?

  5. Re: HR-OS1 3D Models & 3D Printed Armor

    It is just a design, I think the weight is not a problem even if you print with any plastic in the market, but especially with nylon it is like a feather. That is why at the specification of the trossent site they say "Body panels: 3D printed nylon"

  6. #26

    Re: HR-OS1 3D Models & 3D Printed Armor

    I think PLA is even less dense than Nylon.
    I think the real reason is that the default/best plastic on Shapeways is Nylon! (They call it "strong and flexible")

  7. Re: HR-OS1 3D Models & 3D Printed Armor

    But PLA is not as flexible as Nylon and will crack.

  8. #28

    Re: HR-OS1 3D Models & 3D Printed Armor

    ABS is what I use but some of these glow in the dark formulas are well, hum, expermintal lol!

  9. #29
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    137

    Re: HR-OS1 3D Models & 3D Printed Armor

    Quote Originally Posted by dmcman73 View Post
    I had a question regarding the head: Why was this shape chosen over the other shape heads I've seen (like the "traditional" Jimmy head). Was it the weight?
    It's just an aesthetic design I came up with, but I was trying to keep it quite a bit smaller.

    Jimmy, while cute, has an impractically large head. We had a lot of problems with the head cracking like an egg when it would take a hard fall. Furthermore, we don't own the IP to open source the Jimmy 3d models, and the owner of those chose not to release them. I have a few different head designs that should be ready for release in the next week or two though, among some hand variations.

  10. #30

    Re: HR-OS1 3D Models & 3D Printed Armor

    AH, HA! The L-bracket's are for mounting the body shells ;-)
    Should have a full set of black abs skins in a day or so.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Mech Armor
    By ArduTank in forum Mech Warfare
    Replies: 20
    Last Post: 04-29-2014, 09:08 PM
  2. Question(s) motion and measurement models for Kinect
    By ajp in forum Sensors
    Replies: 1
    Last Post: 07-14-2013, 12:34 AM
  3. Destructible Armor?
    By freethinker in forum Mech Warfare
    Replies: 27
    Last Post: 07-30-2012, 04:42 PM
  4. Robot Armor
    By Lightwolf in forum Mech Warfare
    Replies: 3
    Last Post: 06-03-2011, 11:06 PM
  5. Just For Fun Lighter side of Robot models (SFW&NSFW)
    By ashwinmudigonda in forum Off Topic
    Replies: 6
    Last Post: 05-02-2008, 09:15 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •