Results 1 to 2 of 2

Thread: Matrix calculations

  1. Matrix calculations

    Hi all,

    I wanted to ask if matrix calculations can be performed using the Arbotix-M Robocontroller.

    If there is a specific library needed for it, please post a link for it. Thanks.

  2. #2

    Re: Matrix calculations

    Yes, matrix calculations can be performed, by running the appropriate math functions.
    Note that the MCU in the Arbotix-M is very slow (it's an 8-bit MCU with no floating point support running at 16 MHz) so don't expect it to be fast.
    Use whatever matrix library written in C or C++ that strikes your fancy. For 3D math (4x4 homogenous matrices) I like glm.
    Again -- it will run very slow!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Quadruped torque calculations - Confirmation Please!!!
    By Ferret in forum Humanoids, Walkers & Crawlers
    Replies: 25
    Last Post: 07-06-2013, 02:41 AM
  2. Question(s) [Help] build the matrix led with transistor
    By alaterlight in forum Power
    Replies: 0
    Last Post: 01-29-2012, 12:52 AM
  3. Matrix robot walker-with weapons
    By Tymtravler in forum Humanoids, Walkers & Crawlers
    Replies: 2
    Last Post: 04-02-2008, 11:27 AM
  4. Voltage Sensor calculations
    By super-d in forum Sensors
    Replies: 3
    Last Post: 03-01-2008, 11:56 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •