Results 1 to 3 of 3

Thread: hobby pwm micro servo on Arbotix pro

  1. hobby pwm micro servo on Arbotix pro

    got my hr-os1 now assembled ....everythink works fine and now wonder if there is any basic documentation about the Arbotix Pro available....?
    I am interested if it is possible to wire a standard 4.8-6V micro pwm servo to it (actually two like FS90), since I want to built hands/claws for my robot. If not ......is there any ttl micro servo with similar size like the FS90 on the market?

    THX for the answers in advance!

  2. #2
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    141

    Re: hobby pwm micro servo on Arbotix pro

    Arbotix-Pro documentation should be out by the end of the month. There is no PWM servo support in the current firmware and the power going to the IOs is 3.3v.

  3. #3

    Re: hobby pwm micro servo on Arbotix pro

    Woot! Grats. and the Fun begins.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Help Arbotix Robocontroler Hobby Servo ports
    By tiburcio in forum Humanoids, Walkers & Crawlers
    Replies: 2
    Last Post: 03-09-2011, 11:10 PM
  2. Interesting Hack servo v3.00 - Get full PID position and speed control from your hobby servo
    By Antonb in forum Mechanics / Construction
    Replies: 20
    Last Post: 06-27-2010, 10:24 AM
  3. Discussion too tight servo pin spacing on 8 channel micro SSC
    By rslegge in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 03-24-2010, 04:51 PM
  4. Replies: 11
    Last Post: 02-26-2010, 10:57 AM
  5. Hack your Servo V1.00: Make a linear actuator using a hobby servo
    By Antonb in forum DYNAMIXEL & Robot Actuators
    Replies: 4
    Last Post: 01-15-2010, 01:43 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •