Results 1 to 3 of 3

Thread: Sizing and hole patterns for the scoring transponder?

  1. Sizing and hole patterns for the scoring transponder?

    Is there a size and hole pattern drawing somewhere for the older scoring transponder? I have a couple on order but they're awaiting the voltage regulator upgrade. Meanwhile, I'm trying to finalize all mounting holes and sizes for the final go at making the frame of Onyx. Location of tall components and wire connections would be great, too. Also, if there's the same thing for the newer transponders, that'd be good (just to make sure I could hold that if needed.) Finally, the panels themselves (thickness, area, cable locations.) I can kind-of extrapolate from the STLs for the posted 3d printed holders, but I'd prefer an authoritative drawing ;-) And, on that note: I'm seriously considering at least a semi-autonomous mode for aiming. Is bringing a roll of yellow electrical tape for marking good enough, or should I make some kind of clip-on frame? (In two sizes, too...)

    Chuyen thi cong son epoxy gia re, nhan son epoxy tot nhat, Nha cung cap tot nhat https://www.facebook.com/ThiCongSonEpoxyTPHCM.

    tim nguoi giup viec nha

  2. #2

    Re: Sizing and hole patterns for the scoring transponder?

    Yellow tape would probably work.
    If you can find post-its with the entire back covered in sticky, that'd be pretty great.

  3. Re: Sizing and hole patterns for the scoring transponder?

    ok thanks,

    Chuyen thi cong son epoxy gia re, nhan son epoxy tot nhat, Nha cung cap tot nhat https://www.facebook.com/ThiCongSonEpoxyTPHCM.

    tim nguoi giup viec nha

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. What is the hole pattern on the ArbotiX robocontroller?
    By jwatte in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 01-30-2015, 02:20 PM
  2. Question(s) Motor sizing for 4 wheeled robot
    By alphaCentaur in forum Mechanics / Construction
    Replies: 3
    Last Post: 01-22-2014, 12:27 AM
  3. IP Camera stuff (and 2013 scoring transponder)
    By Deimos in forum Mech Warfare
    Replies: 7
    Last Post: 04-07-2013, 05:37 PM
  4. Replies: 0
    Last Post: 01-29-2013, 07:46 PM
  5. Transponder Rev. B question
    By CogswellCogs in forum Mech Warfare
    Replies: 3
    Last Post: 12-06-2011, 09:49 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •