Results 1 to 2 of 2

Thread: CM-510 (Bioloid Premium) serial connection to BeagleBone Black (BBB)

  1. #1
    CarAlAg Guest

    CM-510 (Bioloid Premium) serial connection to BeagleBone Black (BBB)

    Hello. I need help in how to understand and making work a serial connection between a BBB and a CM-510.

    Any idea? Has anybody had to face this very issue?

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,317
    Images
    27
    Rep Power
    282

    Re: CM-510 (Bioloid Premium) serial connection to BeagleBone Black (BBB)

    Easiest way would probably be to get a Robotis LN-101 dongle to connect the 4-pin zigbee port of the CM-510 to a USB port on the BBBk. If the BBBk uses 5V/3.3V-safe logic, then you may be able to connect the zigbee port directly to one of the UARTs of the BBBk. The 4-pin zigbee port should be using JST PH series connectors and the pin numbering/naming should be somewhere on the Robotis support site for the CM-510 and/or the ZIG-110. You would then use the RoboPlus Task Remocon() functions to send signed 16-bit values between the CM-510 and BBBk.


    If you feel comfortable with C/C++, then you may be able to use the Robotis provided libraries for controlling the CM-510 via programs compiled with avr-gcc. I used part of the Robotis libraries to make some 'easy functions' for the CM-510/700 and CM-530 a while back, but have not touched them in quite a while.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. BeagleBone Black for Mech
    By bloftin in forum Mech Warfare
    Replies: 17
    Last Post: 02-04-2017, 07:30 PM
  2. Question(s) OPENCM9.04 with raspberry pi ROS using serial connection
    By Nico in forum Arbotix, Microcontrollers, Arduino
    Replies: 4
    Last Post: 06-03-2014, 08:51 AM
  3. BeagleBone Black - starting to play...
    By KurtEck in forum Robot Computers
    Replies: 65
    Last Post: 09-02-2013, 11:22 AM
  4. Beaglebone Black now available
    By Grumpybeard in forum Arbotix, Microcontrollers, Arduino
    Replies: 12
    Last Post: 04-26-2013, 01:45 PM
  5. Lassen GPS Eval kit and serial connection
    By IntoMo in forum Sensors
    Replies: 2
    Last Post: 06-30-2008, 11:24 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •