Page 1 of 2 12 LastLast
Results 1 to 10 of 16

Thread: Beginnings of ROS on the HROS-1/Hello from University

  1. Beginnings of ROS on the HROS-1/Hello from University

    Hi all,

    Sorry for not formally introducing ourselves earlier. I'm part of a university team with 5 of the HROS-1 robots. To give you a quick update of our progress, we worked through all of the available code, expanded the scope of node server to call commands and monitor progress on the web, implemented the face detection algorithm in openCV and wrote a Python wrapper to call the rme poses outside of running the program.

    Since we seemed to have tapped out the capability of the software that currently exists (and we wanted to continue to do cool things) we've decided to start integrating the system with ROS for HROS-1. We've got Indigo installed on Desktop and RPi's (in the robots), and communication working between nodes on different machines. Currently, we're trying to use the Arbotix Pro Controller with the existing ROS library for it, seen here: http://wiki.ros.org/arbotix?distro=indigo

    So a few problems that we've run into:
    1. There's no documentation on the Arbotix Pro Robocontroller that's in the HROS-1. At least, we haven't found any yet. Is this custom made for these robots? If not, does anyone have experience/more details on it.

    2. We are currently trying to run the controller with the existing code for the Arbotix Terminal (part of the ROS Arbotix Stack). This should allow us to view and assign servos detected by the board. Currently, we're working with the board outside of the robot, directly hooked up to the desktop running Linux/ROS and we're trying to hook one servo at a time so it assigns an ID to the servo. We're able to run a program that looks for the servos but it never identifies any. This program (http://wiki.ros.org/arbotix_python/T...%20Servo%20IDs) is our example and we should be seeing a "1" when we run it with one of the servos but we just get "..." the entire time.

    Does anyone have any experience with the robocontroller or ROS and have any ideas how to help us out. We think we'd be able to move pretty quickly to controlling the HROS-1 from a higher level if we could figure this out.

  2. #2
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    35

    Re: Beginnings of ROS on the HROS-1/Hello from University

    Quote Originally Posted by Piper View Post
    Hi all,

    Sorry for not formally introducing ourselves earlier. I'm part of a university team with 5 of the HROS-1 robots. To give you a quick update of our progress, we worked through all of the available code, expanded the scope of node server to call commands and monitor progress on the web, implemented the face detection algorithm in openCV and wrote a Python wrapper to call the rme poses outside of running the program.
    Hi Piper!

    You all have been busy I'm curious if/what you've done with the OpenCV data, possibly keep the robot's head looking towards a detected face?

    Good going on getting up speed with ROS. I wish I had some helpful information but I'm in a bit of a holding pattern for a little while. Anyway, can't wait to see what you guys come up with.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  3. #3
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,315
    Images
    27
    Rep Power
    279

    Re: Beginnings of ROS on the HROS-1/Hello from University

    The arbotix library is completely incompatible with the arbotix-pro, and the installation instructions for 'arbotix_firmware' are still incredibly out of date. Everything for arbotix/arbotix-m has been moved to github. None of the code.google files should be used for the arbotix or arbotix-m as they are quite old and kept alive only for reference.

    The first round of beta HR-OS1 have arbotix-pro that are essentially clones of the CM-730 with some changes to layout, and I'm thinking there were a couple small changes to the firmware regarding the LEDs. Hoping the second round of HR-OS1 get the newer revision of Arbotix-Pro with the reworked TTL and RS-485 buss connections that can safely coexist (like the CM-700, instead of mutually exclusive design of CM-730). The CM-730/Arbotix-Pro simply behave as a dynamixel device and pass-through with an on-board FT232RL USB2UART IC. The FT232RL connects to one UART, the CM-730/Arbotix-Pro processes any commands for itself (read/write), then passes it on to the primary dynamixel buss of the servos.

    Unfortunately, the CM-730 firmware does not implement a pseudo-'sync_read'/'bulk_read' like the USB2AX and regular arbotix to get around the USB timeout issues of using multiple AX-compatible 'read' commands. It is probably something I will work on when I get an arbotix-pro, since taphi expects a lot of position/velocity/effort feedback from the servos and AX-series servos do not implement the actual 'sync_read' and 'bulk_read' commands of the MX-series and Dynamixel Pro servos.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  4. #4

    Re: Beginnings of ROS on the HROS-1/Hello from University

    None of the code.google files should be used for the arbotix or arbotix-m as they are quite old and kept alive only for reference.
    Delete them all, check in a README.txt that points at GitHub...

  5. #5
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    Re: Beginnings of ROS on the HROS-1/Hello from University

    Quote Originally Posted by Piper View Post
    Hi all,

    Sorry for not formally introducing ourselves earlier. I'm part of a university team with 5 of the HROS-1 robots. To give you a quick update of our progress, we worked through all of the available code, expanded the scope of node server to call commands and monitor progress on the web, implemented the face detection algorithm in openCV and wrote a Python wrapper to call the rme poses outside of running the program.

    Since we seemed to have tapped out the capability of the software that currently exists (and we wanted to continue to do cool things) we've decided to start integrating the system with ROS for HROS-1. We've got Indigo installed on Desktop and RPi's (in the robots), and communication working between nodes on different machines. Currently, we're trying to use the Arbotix Pro Controller with the existing ROS library for it, seen here: http://wiki.ros.org/arbotix?distro=indigo
    As others said, that package is not compatible with the Arbotix-Pro. It's outdated and written for the Arbotix-M specifically. We do have a project in the works that will create a specialized firmware for the Arbotix-Pro and accompanying ROS package, but I cannot give you an eta on that currently.

    The new Arbotix-PRO ROS firmware will not be compatible with the existing CM730-based firmware that is used in the Darwin-OP/HROS1-Framework.


    Quote Originally Posted by Piper View Post
    So a few problems that we've run into:
    1. There's no documentation on the Arbotix Pro Robocontroller that's in the HROS-1. At least, we haven't found any yet. Is this custom made for these robots? If not, does anyone have experience/more details on it.
    It was custom made for this project, and is still in beta as well. This is the reason we do not yet sell the Arbotix-Pro by itself (along with waiting on our contract manufacturer to finish our latest batch). However, the reason the Wiki points to the CM730 documentation is because almost all of it is directly applicable. The Arbotix-Pro was built to be a drop-in clone replacement for the CM730, so please refer to the Darwin-OP documentation on the CM730 for more info: http://support.robotis.com/en/produc...r_(cm-730).htm

    There is also software documentation that details the CM730 libraries within the framework.

    Quote Originally Posted by Piper View Post
    2. We are currently trying to run the controller with the existing code for the Arbotix Terminal (part of the ROS Arbotix Stack). This should allow us to view and assign servos detected by the board. Currently, we're working with the board outside of the robot, directly hooked up to the desktop running Linux/ROS and we're trying to hook one servo at a time so it assigns an ID to the servo. We're able to run a program that looks for the servos but it never identifies any. This program (http://wiki.ros.org/arbotix_python/T...%20Servo%20IDs) is our example and we should be seeing a "1" when we run it with one of the servos but we just get "..." the entire time.
    Please use the provided dxl_monitor within the HROS1 Framework to assign servo IDs and make changes. To reiterate for others reading through this thread: The existing ROS Arbotix Stack is NOT compatible with the Arbotix-Pro. There will be a separate ROS Arbotix-PRO package and firmware to be released later this year. The architecture between the Arbotix-M and Arbotix-Pro is entirely different.

    Quote Originally Posted by Piper View Post
    Does anyone have any experience with the robocontroller or ROS and have any ideas how to help us out. We think we'd be able to move pretty quickly to controlling the HROS-1 from a higher level if we could figure this out.
    Unless you intend to design the entire control system and IK/walking gait from the ground up, I suggest you look into the ROS/Darwin-OP projects that are available online. These simply wrap the existing Darwin-OP Framework into a ROS package, which is the simplest way to integrate ROS to the HROS1. HumaRobotics recently posted a pretty good writeup on their integration of the Darwin-OP to ROS, which would serve as an excellent starting point. There are also a few other projects out there that do something similar.

    http://www.generationrobots.com/en/c...gazebo-and-ros

    Another research group: http://wiki.iri.upc.edu/index.php/Darwin_installation

    http://wiki.iri.upc.edu/index.php/DarwinRobot

    http://wiki.iri.upc.edu/index.php/IriDarwin

    We have created a small hand-picked development group that is working on implementation of ROS on our Hexapods & Humanoid platforms, however the current focus is finishing the hexapod project before moving towards humanoids. The HR-OS1 will stay based around current framework and be integrated into ROS similar to how Huma has implemented this, while the HR-OS5 will use that as an intermediary step with the eventual goal of moving it entirely away from the Darwin-OP based framework and towards a pure-ROS implementation. I can make no guarantees on the release dates of these projects though, as this work is very time consuming.

  6. Re: Beginnings of ROS on the HROS-1/Hello from University

    Hey all,
    Thanks for the advice. Two questions now:
    1.) If we're gong to write a wrapper for the existing HROS-1 Framework, do you have any suggestions of where to start working within it?
    2.) If we do go ahead and do this, integrating as much into ROS as possible, do you think it will all be for naught when the new framework eventually comes out? Or will the new framework for ROS be able to fit in with whatever we've written by then. I guess that's kind of a case-by-case thing depending on our approach but I figured I'd see if you all have any thoughts.

  7. #7
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    Re: Beginnings of ROS on the HROS-1/Hello from University

    Quote Originally Posted by Piper View Post
    Hey all,
    Thanks for the advice. Two questions now:
    1.) If we're gong to write a wrapper for the existing HROS-1 Framework, do you have any suggestions of where to start working within it?
    2.) If we do go ahead and do this, integrating as much into ROS as possible, do you think it will all be for naught when the new framework eventually comes out? Or will the new framework for ROS be able to fit in with whatever we've written by then. I guess that's kind of a case-by-case thing depending on our approach but I figured I'd see if you all have any thoughts.
    1) I believe the solutions I linked you wrap the entire Darwin-OP framework. If you're looking for more information on how the library is initialized and a basic teleoperation demo, check the ps3_demo or the node_server projects.
    2) We intend on looking at the two solutions I had linked and seeing how they tied into the Darwin-OP framework, and likely using one or both as a starting point for the integration. We've only just now started work on this, so too early to give you many details.

    My goal for the ROS_Humanoid project is to make an open, flexible ros package that can handle a number of configurations (OS1, OS5, Darwin, Bioloid).

    There will be two phases:

    1) Wrapping the existing HR-OS1/5 framework into a ROS package. This allows us to keep our existing work and add ROS packages on top of it. We might eventually break out the Darwin walking IK/gait out into it's own package within the project and implement a better control/motion package than the current Darwin "Action" module (which is not great) and replace it with something KDL or Moveit Based. This Phase 1 project will be based around the existing Arbotix-Pro CM730 firmware and HROS1/5 Framework. Those steps would be in preparation for phase 2:

    2) Complete move away from the Darwin-OP based framework, and implementation of ZMP based walking gait. A 'pure' ROS implementation if you will. This will be where our project splits into two separate code bases for the OS1 and OS5. The OS1 will stay behind with whatever we come up with for it in Phase1, while the OS5 will branch away into the Phase 2 code project with ZMP, and take advantage of the new Arbotix-Pro ROS firmware and package. The OS1 doesn't have the physical hardware capable of a ZMP gait. so it will likely stay based on the Darwin-OP framework.

    So within the context of Phase 1, I doubt any of your efforts would be for naught. Once we get a bit more off the ground with Phase 1 (over the next 30 days or so) we invite you to collaborate with us on the execution of it. Perhaps we can avoid reinventing too many wheels.

  8. Re: Beginnings of ROS on the HROS-1/Hello from University

    What worries me about the current HR-OS1 framework is that it is licensed with the GPL, which means that any software that links to it also has to be GPL.

    The ROS community prefers liberal licenses so that individuals and companies are unrestricted in what they can do with the software.

    If you made a ROS framework for the HR-OS1 and other robots, could you at least give the message files a non-copyleft license so that people are free to integrate their software with your robots without restriction?

  9. #9
    Join Date
    Dec 2007
    Location
    Portland, OR
    Posts
    3,198
    Images
    952
    Rep Power
    142

    Re: Beginnings of ROS on the HROS-1/Hello from University

    Quote Originally Posted by jdddog View Post
    What worries me about the current HR-OS1 framework is that it is licensed with the GPL, which means that any software that links to it also has to be GPL.

    The ROS community prefers liberal licenses so that individuals and companies are unrestricted in what they can do with the software.

    If you made a ROS framework for the HR-OS1 and other robots, could you at least give the message files a non-copyleft license so that people are free to integrate their software with your robots without restriction?
    Unfortunately we don't have any control over the license of the HR-OS1 Framework. I asked ROBOTIS what the Darwin-OP framework was released under, they came back and said GPL was okay... then later revised that to LGPL. Since I had already released the code under GPL and they haven't ever placed an official public license on the code, I told them I intended to keep the original license it was released under (as none of my code uses what they wanted under the LGPL).

    I don't think this is much of an issue, worst case the wrapper package around the OS1 framework would need to be GPL, but anything in addition to that can be whatever we choose. I likewise would prefer to keep things in line with BSD.

  10. Re: Beginnings of ROS on the HROS-1/Hello from University

    Cool.
    We have a group working on these robots over the summer, mostly with the intent of getting them sufficiently operational. We'll start classes up again at the beginning of September and at that point, we'll be trying to use the HROS-1 in some capacity for our school's engineering design projects. In some sense, we'd love to have at least some ROS functionality at that point and start to work on higher level things/real applications. Obviously, full ROS integration won't be done at that point and the ROS wrapper will still be a work in progress (on your guys' part). We will continue reading up this weekend on methods for writing wrapper and we'll try to keep you all posted on our progress. Let us know how you're doing to, and hopefully we can collaborate a little more fully when y'all have finished the Hexapod work in a few weeks. Good luck!

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Writing on a board with HROS-1 using inverse kinematics
    By Weebo in forum Humanoids, Walkers & Crawlers
    Replies: 3
    Last Post: 06-17-2015, 03:29 PM
  2. Question(s) University Senior Project-Xbee?
    By bcompto5 in forum Robotics General Discussion
    Replies: 0
    Last Post: 09-26-2010, 12:11 AM
  3. University graduate robotics programs
    By Resilient in forum Robotics General Discussion
    Replies: 16
    Last Post: 04-11-2009, 06:41 PM
  4. Sample University Proposal
    By Firestorm65 in forum Mech Warfare
    Replies: 10
    Last Post: 02-05-2009, 09:49 AM
  5. Replies: 23
    Last Post: 08-02-2008, 11:51 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •