Results 1 to 2 of 2

Thread: Arbotix-Pro doesn't recognize servos

  1. Arbotix-Pro doesn't recognize servos

    Hi everyone,

    Recently the Arbotix-Pro board on one of our robots stopped working for an unknown reason. The robot was working perfectly fine, running the PS3 demo and walking. After one rather "normal" fall, the robot wouldn't move anymore.

    We tried to replace the Arbotix-Pro board with one from another robot and everything was back to normal. So I imagine the problem is in the board, although I don't know what it might be exactly.

    This is the output from the dxl_monitor:

    Click image for larger version. 

Name:	Arbotix PRO - Feedback.jpg 
Views:	211 
Size:	97.4 KB 
ID:	6087

    Any ideas of what might have happened?

    Thank you in advance.

  2. #2
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    278

    Re: Arbotix-Pro doesn't recognize servos

    Can it find any servos when testing with spares? It is possible that the impact caused issues with a solder joint somewhere in the dxl communications ICs, specifically the read enable. Also possible that something inside the chassis shorted one of the dxl ICs during the impact. If you have a logic analyzer, try searching for servos while monitoring the TX and RX pins of the DXL UART at the STM32, the TX enable and RX enable pins, and the DATA line at the DXL connectors. The schematic is at the Interbotix github 'ArbotixPro' repo.

    edit: Another possibility is that the 5V voltage regulator got damaged, which would cut power to the TX side of the DXL ICs and the RPi2. Much easier to check that the 5V supply is still functioning than hooking into the DXL ICs if everything stopped working.
    Last edited by tician; 07-08-2015 at 04:01 PM.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Arbotix controlling different servos
    By Salman in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 09-06-2014, 04:25 PM
  2. arbotix robocontroller servos not recognized
    By bellscotcv in forum Arbotix, Microcontrollers, Arduino
    Replies: 9
    Last Post: 07-17-2012, 11:56 PM
  3. Question(s) EX-106 servos with arbotix
    By tduv in forum Robotics General Discussion
    Replies: 14
    Last Post: 05-29-2012, 01:57 PM
  4. Question(s) EX-106 servos with arbotix
    By tduv in forum Project Showcase
    Replies: 0
    Last Post: 05-26-2012, 12:50 PM
  5. Question(s) Controlling AX or RX servos using arbotix
    By darkback2 in forum Software and Programming
    Replies: 34
    Last Post: 11-11-2011, 10:05 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •