Results 1 to 7 of 7

Thread: New mechwarfare build concept

  1. #1
    Join Date
    Jul 2015
    Location
    Stafford, Va
    Posts
    11
    Rep Power
    16

    New mechwarfare build concept

    Hello everyone, I'm starting to design a new mechwarfare competitor. Check out my idea's and give me advice on how I can make it better and more viable.

    I know very very little about robotics but I'm learning more everyday. At this point I want to get my idea's out into the community and see what the responses are to see if I'm going in the right direction. I don't want to invest in a micro controller and servo's until I'm sure that they are the right ones for the job.

    I wanted to make a mechwarfare capable version of Stanford's isprawl. I thought it was hydraulically driven, but it turns out its not. Its hard to describe what it does use so here's a youtube url of a very similar robot, and it describes how it works. /watch?v=SMlIoYvWUOU

    Now I know I'l need a microcontroller, I know I'l need a custom drive train cnc'ed, I know I'l need an electric motor to run the drivetrain, I know I'l need 6 servo's to position the angle of the legs , And I know I'l need somekind of wireless video and wifi control. ( wireless video and wifi control I know verrrrrry little about, I've been searching the threads for info on the basics but I've had no luck, please help) I'l also need to come up with some type of springy material to use as the hip joints. I know where to get the metal wires for the leg actuation.
    I know of a 3d printing service near me so I'l use that for the frame.

    I plan on making the exterior torso of the mech look like this, only with 6 legs (the legs will have to look completely different), and it will have to have the metal actuating wires run out of the body, around, and then down into the legs. I could carve the exterior out of balsa wood, or use 3d printed parts if its light weight enough. The metal actuating cables would block the gun from having more than maybe 50 degrees of motion, so the left and right motion of the gun and camera will be limited, but the up and down motion would be unaffected. I would like to use a mouse for control of the gun/camera turret. I might use a custom plastic version 2 (m16/m4) or version 7 (m14) aeg gear box with a dual sector gear for high rate of fire/low fps, and might use feeding system like one out of a aeg ak drum mag (auto winding) so that I can store the bb's in the body and not in an exterior hopper like I see some of your mechs use. Would love to sculpt a shroud for the barrel that looks like a mini gun.
    Click image for larger version. 

Name:	doodle.png 
Views:	616 
Size:	357.2 KB 
ID:	6088
    If anyone has any ideas, any ideas at all, on which microcontroller, motor, servo's I could or should use, I'd really appreciate the tips.
    Also, how can I get started learning wifi control and video transmission. I don't even know what to call it? Is it called ip/tcp control? What kind of hardware and software do most mechs use for that?
    Is there anything else I should learn up on that I've missed touching on to really make this project top notch?

    Thanks
    -Carl Gustav
    Last edited by Carl Gustav; 07-14-2015 at 01:53 PM.

  2. #2
    Join Date
    Jul 2015
    Location
    Stafford, Va
    Posts
    11
    Rep Power
    16

    Re: New mechwarfare build concept

    I know that iSprawl uses cirrus CS-5.4 servo's.
    isprawl weighs 315grams or .69 pounds.
    I'm guessing my mech will be atleast 3 times that weight, so I'l need servo's with more torque and holding power.
    I plan on sparing no expense so maybe one of the dynamixel offerings will work well. I wonder if there are any robot servos that are smaller, lighter, faster, and torque-y-er than dynamixels.

  3. #3

    Re: New mechwarfare build concept

    You may get slightly cheaper servos from Dongbu instead of Robotis. For robotics, you're unlikely to find anything "better" from the RC hobby crowd, and from the motion control / industrial automation crowd, you'll likely to find much heavier and more expensive stuff.

    The best "bang for buck" in robotics servos is likely the MX-64. For less money, and less capability, the AX-12A and the DRS-0101 are probably good alternatives.

    Btw: the Japanese insect walker you described may violate the Mech Warfare rules in two ways:
    1) It has more than four legs
    2) It uses a cam-driven locomotion system (there's a cam that drives the actuation wires that drives the pistons that bounce it forward.)

  4. #4
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    279

    Re: New mechwarfare build concept

    While there is a class that permits 6 legs ('open'? league), I don't think it has ever actually been supported in any of the official competitions due to lack of entrants. The only league guaranteed to have actual battles at any official event would be the standard/regular (no more than 4 legs) league. There might be support for 'hardcore' league battles if the venue has a sufficiently safe arena/enclosure and any entrants actually show up.

    Yep, the isprawl design almost certainly violates the 'no cam' drive system by powering more than one leg with a single actuator. Might be able to get away with one driving motor plus cam (converting rotation to reciprocating motion) per leg extension 'joint' and using cheap servos for steering the legs, but I think it is very unlikely that a single driving motor with one cam to control all the leg extension 'joints' using bowden cables would be legal. So instead of one continuous rotation motor and four/six servos to control leg vectoring, you would have to have four legs with each leg consisting of one continuous rotation motor with its own cam (or just use a normal servo) to drive one bowden cable leg extension and one servo to control leg vectoring for a minimum of eight standard servos (or four standard servos and four individually driven continuous rotation motors/servos each with its own cam).

    iSprawl's predecessor, aquasprawl, used single action hydraulic cylinders for each leg, but that limited the retraction speed. Better version would have used double action cylinders for each leg and two of the 'drive'/'master cylinders' 180 degrees out of phase (or just swap input and output ports).


    Was thinking about constructing a prototype/minimalist 'Jamie' (GITS:SAC Jameson chassis) from my 'spares'/'why did I buy this again?' supply of eight HXT900 servos to control pitch and roll of each leg then using pololu/sanyo micro gearmotors to control the lead screw that turns each leg into a linear actuator. It would operate quite a bit like iSprawl except each leg extension would be individually controlled by a single gear motor, there would be two degrees of freedom in each leg vectoring for higher maneuverability/dexterity, and it would be much slower because of the lead screw mechanism.
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  5. #5
    Join Date
    Jul 2015
    Location
    Stafford, Va
    Posts
    11
    Rep Power
    16

    Re: New mechwarfare build concept

    I forgot that the hexapod class almost never has any entries. I guess I didn't really think that that design would be considered cam driven, but it totally is.
    Good thing you guys told me that before I spent a ton of money of cnc'ing.
    I guess its back to a hydraulic quadruped then.

    /watch?v=l6mNK5pqZ4Y
    ^What do you guys think about this robot? Have you ever seen it before?

  6. #6
    Join Date
    Sep 2010
    Location
    ಠ_ಠ
    Posts
    2,313
    Images
    27
    Rep Power
    279

    Re: New mechwarfare build concept

    If each extension/cable is controlled by a single, independent motor/servo, then it would very likely be acceptable. The 'no cam' rule is intended to restrict walkers like the strandbeest and attacknid that use a single, continuously rotating motor to drive multiple legs through a cam/linkage system instead of independent control over each leg. You can have linked control over certain joints of multiple legs (e.g. one servo that controls yaw/roll of two legs), but it is the 'driving multiple legs with one continuous rotation motor' that is verboten. There are designs like 'twitch' that use very few servos to control multiple legs/feet, but their statically stable design (three feet per 'leg') prevents them qualifying as true bipeds.

    Had not seen that little hydraulic walker, but quite nice. Almost certainly uses custom machined manifold, valves, and cylinders, and probably the pump as well (cheap pumps can be found, but not sure how long they would withstand exposure to non-water liquids).
    Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
    "You have failed me, Brain!"
    [git][mech][hack]
    gives free advice only on public threads

  7. #7

    Re: New mechwarfare build concept

    THAT is a cute walker :-)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. MechWarfare entry HD2
    By Janis in forum Mech Warfare
    Replies: 17
    Last Post: 04-19-2013, 06:32 AM
  2. Awesome Micro/Mini Robot Concept Designs
    By jeppers113d in forum Robotics General Discussion
    Replies: 1
    Last Post: 01-06-2011, 10:52 AM
  3. Arena Concept
    By dalocogamer in forum Mech Warfare
    Replies: 5
    Last Post: 07-05-2010, 02:04 PM
  4. Project Concept----ideas?
    By Redhammer in forum Software and Programming
    Replies: 7
    Last Post: 12-05-2009, 03:15 PM
  5. Most insanely cool game concept I've ever seen!
    By Adrenalynn in forum Off Topic
    Replies: 9
    Last Post: 08-04-2008, 01:19 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •