Results 1 to 2 of 2

Thread: Does WidowX work with ROS arbotix_python?

  1. #1
    RoBoCeRo Guest

    Question Does WidowX work with ROS arbotix_python?

    Hi,

    I've been testing the arm with arbotix_python and it seems not to work very well with the MX dynamixels. You can read and write but it doesn't correspond with the desired/read position.

    Thanks,

  2. #2
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    35

    Re: Does WidowX work with ROS arbotix_python?

    I've not used the arbotix_python ROS package but looking at the wiki and based on your description of the problem I would first guess you haven't set the "ticks" parameter.

    Code:
    ~dynamixels/<servo>/ticks (int, default: 1024)
    
    • Number of ticks, for EX-106s, you would pass in 4096, other servos likely won't need this altered.
    If this is true you'll also want to change the neutral, range, ticks, min_angle, max_angle, max_speed parameters to match your MX servos. http://wiki.ros.org/arbotix_python#Parameters
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Request WidowX Arm Position?
    By LukeM in forum Interbotix Robotic Arms
    Replies: 2
    Last Post: 01-08-2017, 08:21 PM
  2. Example yaml file for arbotix_python io sensors?
    By Pi Robot in forum ROS - Robot Operating System
    Replies: 7
    Last Post: 02-06-2014, 09:07 AM
  3. Question(s) Just Received WidowX Arm
    By mcintosh in forum Interbotix Robotic Arms
    Replies: 12
    Last Post: 12-19-2012, 11:46 PM
  4. Getting arbotix_python diff_controller to hold a straight line
    By Pi Robot in forum ROS - Robot Operating System
    Replies: 3
    Last Post: 12-23-2011, 10:14 AM
  5. new b! i need help please!! cant get it to work
    By openmindedjjj in forum Robotics General Discussion
    Replies: 11
    Last Post: 06-28-2008, 08:35 AM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •