We've decided to start our Black Friday Sale early this year - 20% off all of our InterbotiX and RobotGeek products, and 10% of the rest of the catalog. The sale will be live by today at noon Central time (in the next 2 hours). The sale will be automatic, so you won't need a coupon for the 10-20% off.

I've also created a special coupon for the first 10 forum members who want to use it. The following coupon code will get you free UPS ground shipping on your order in addition to the normal sale.
Code:
trcblf1
I'm also going to include a tiny 3d printed hexapod for as many forum members as I can print out between now and monday. If you're not one of the first 10 to use the coupon, just put a note in the comments and I'll put a tiny hexapod in if we still have any.

If you have any issues with the code or sale, let me know at [email protected]

Thanks everyone, and happy Thanksgiving!