Page 1 of 3 123 LastLast
Results 1 to 10 of 24

Thread: mAh or C. Which is more important?

  1. mAh or C. Which is more important?

    Hello, given two batteries: Battery A has more mAh (e.g. 2000) than Battery B. However, its C value is lower. The mAh*C values are almost the same. Which battery do you recommend and why? Thanks.

  2. #2
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    41

    Re: mAh or C. Which is more important?

    mAh tells you the capacity of the battery and the C rating or continuous discharge rating tells you how much current the battery will be able to supply to your project.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

  3. #3

    Re: mAh or C. Which is more important?

    If the C rating of battery A is good enough for your application, then the higher capacity is going to give you more runtime.

    However, I would expect battery A to weigh more, which may or may not be a consideration for you.

  4. Re: mAh or C. Which is more important?

    Thank you. How can I tell if the C rating is good enough or not? I recall somebody mentioning that it is better to get a battery with higher mAh*C value. Is that right?

  5. #5
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    87

    Re: mAh or C. Which is more important?

    It depends on how much current you need. Like jwatte said, batt A will give you longer runtime since it has more energy. But if weight is important batt B might be a better choice. In general it's better to have a battery that can deliver more current.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  6. #6

    Re: mAh or C. Which is more important?

    If I recall, 1C is the milliamps that the battery can put out in 1 hour. For example, if you had a 1000mAh battery then 1C is 1000mA or 1 amp. If you had a 2000mAh battery then the same 1C rating would provide 2 amps of continuous current. The C rating by itself is meaningless without also factoring in the mAh rating.

    You need to determine how many amps your project needs at max load and then get a battery that has at C rating that will provide at least that much power. As long as the C rating is high enough, going for a C rating higher than you need doesn't give you anything extra. When choosing a battery, I usually determine how much current I need then then find the largest battery based on mAh that will fit in the available space.

  7. #7

    Re: mAh or C. Which is more important?

    How can I tell if the C rating is good enough or not?
    How long do you need to run? Rate the battery for enough mAh that it can sustain the average current for at least that long.

    How much current will your motors/servos/controllers/equipment draw? On average? At peak?
    Rate the battery so that the C rating times mAh capacity divided by 1 hour is at least twice the average draw, and higher than the peak draw.

    Now, you probably realize that the battery is too heavy, so you have to compromise on runtime, and re-do the math (to reduce weight, lower the mAh, increase the C to compensate for draw.)

    For most robots, 10 C is a fine rating, and most hobby/RC batteries you get these days are more than that anyway. High C ratings are mainly for very high peak draw applications, like big brushless motors in RC cars, or quadcopter fliers.

  8. #8
    Join Date
    Jul 2012
    Location
    Richmond, IN
    Posts
    652
    Rep Power
    47

    Re: mAh or C. Which is more important?

    Quick example: HS Walker ran on a 20C 2200mAh battery, and only killed it because of being left on

    However, my twin engine RC aircraft requires at minimum a 2200mAh 30C LiPoly (2.2Ah X 30C= 66A continuous draw)
    The twin runs 30A power packs (motor+ESC) the 5000mAh I put in it is just bonus cap so I can fly for more than 7-10 min at a time.


    The batt for HS Walker only cost me $20. (Will give link if asked)

  9. Re: mAh or C. Which is more important?

    Thanks for the replies. I have two confusions. First, should I choose a battery with higher mAh or higher mAh*C. From this thread, it seems that mAH is more important especially when C is over 20. Am I right? Second, in the past, I read that higher C batteries mean they run out quickly due to larger discharge rate. So, this is incorrect?
    Last edited by Snoopy; 08-08-2015 at 09:00 PM.

  10. #10
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    87

    Re: mAh or C. Which is more important?

    No, two batteries with the same mAh but different C will run out at the same time under the same discharge current. The only difference is that the one with higher C can deliver even more current. Still they will have the same amount of energy (wattage).
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. One more thing about SSC-32...Important
    By ahmed in forum Arbotix, Microcontrollers, Arduino
    Replies: 18
    Last Post: 10-20-2008, 12:18 PM
  2. Interesting 10 Important Differences Between Brains and Computers
    By Matt in forum Robot Computers
    Replies: 5
    Last Post: 04-08-2008, 01:44 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •