Page 2 of 2 FirstFirst 12
Results 11 to 14 of 14

Thread: Learning ROS ++

  1. #11
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    80

    Re: Learning ROS ++

    Thanks for your input jwatte and Kurt!
    Sounds like I should be good then.

    My XU4 came with Ubuntu 15.04 so I'm going to replace it with the 14.04.1 20150212 image. I assume that is the correct one for making ROS work properly.
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  2. #12

    Re: Learning ROS ++

    As I am running Ros Indigo and not Jade, I am running off of the 14.04.1, latest image, I then do all of the stuff to update it to the latest stuff:

    sudo apt-get update
    sudo apt-get upgrade
    sudo apt-get dist-upgrade

    I then run the odroid utility:
    sudo odroid-utility.sh

    And in there I update all of the kernel components. (I also on the first boot also use this utility to setup to use the whole space on the emmc.

    I have also followed many of the steps for building up my ROS image as murrman did in the posting: http://forum.odroid.com/viewtopic.php?f=95&t=7446

    In particular I am using the older version of ROS indigo that he uses here and not the more up to date version that listed as the official version up at: http://wiki.ros.org/indigo/Installation/UbuntuARM As I have found that some components like Robot Publisher faults on startup in the official repos...

    From the Odroid Ros Image by murrman, building some of the other components from sources can take quite a bit of time and can eat more memory than you have, so I typically setup a swap area for my Odroid. To do this I use the quick method that is shown in: https://www.digitalocean.com/communi...n-ubuntu-14-04

    Good Luck!

    Kurt

  3. #13
    Join Date
    Jan 2008
    Location
    Norway, Stavanger
    Posts
    790
    Images
    276
    Rep Power
    80

    Re: Learning ROS ++

    Thanks for the guidance Kurt. This evening didn't go so well. It looks like I need to get a proper microSD USB adapter first.. I think I've one at work that might work.
    Last edited by Zenta; 09-06-2015 at 05:26 PM. Reason: Typo on phone..
    Kåre Halvorsen aka Zenta
    ---------------------------------
    Zenta's YouTube channel
    Zenta's Blog
    Zenta's Instagram

  4. #14
    Join Date
    Mar 2015
    Location
    Texas
    Posts
    342
    Images
    15
    Rep Power
    34

    Re: What DC-DC converter do you use for Odroid?

    Quote Originally Posted by Zenta View Post
    I'm a bit unsure what DC-DC converter I should use. So far I've tried the Turnigy 8A UBEC. I'm a bit worried about the 5,17 - 5,2v output though. I posted a Q about it on the Odroid forum and the answer I got was that it should probably be OK.

    I'm a bit irritated about the voltage output isn't stable 5.0v though. What I recall reading from this forum some of you are using the Pololu 5V, 5A Step-Down Voltage Regulator D24V50F5? from this post on the Odroid forum it looks like the Pololu 5V, 9A Step-Down Voltage Regulator D24V90F5 might be a better solution?

    The thread starter ended up with a rather low-cost converter. I feel that one is a bit large when it comes to size and weight..

    My main question of this post is, what DC-DC converter are you using and what are the voltage readings?, and other suggestions are welcome.
    With the XU3 on ROSie I've been using the 5V 5A step down regulator from Pololu with no problems https://www.pololu.com/product/2851

    The voltage reading was about 4.95V.
    01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011

    My Instagram
    My YouTube

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. my learning build
    By Warsloth in forum Robotics General Discussion
    Replies: 31
    Last Post: 06-27-2013, 02:26 PM
  2. Learning with the Bioloid
    By badpanda in forum Humanoids, Walkers & Crawlers
    Replies: 12
    Last Post: 04-09-2013, 08:47 PM
  3. Programming - help learning
    By mblackwolf in forum Software and Programming
    Replies: 2
    Last Post: 11-25-2011, 11:15 PM
  4. Question(s) Learning embedded
    By Resilient in forum Robot Computers
    Replies: 6
    Last Post: 12-18-2008, 02:03 PM
  5. Learning Electronics
    By jes1510 in forum Robotics General Discussion
    Replies: 12
    Last Post: 12-06-2008, 12:12 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •