Hi,
First, I'm a total noob when it comes to Linux and ROS, but my goal is to learn. Due to little free time my progress will certainly be slow. To be honest I'm a bit frustrated since I've tried writing a lot and suddenly I hit the back button or something and all text are gone, sigh..
A couple of days ago I just finished our 5. outdoor project this summer.
Our 4. project was a new stair.
I've told my wife I'm going to spend some time with my robots too this Autumn..
So far I'm still torn between a mcu or a mini computer solution. I do like the old BAP and the newer Teensy3.1. Actually, I soldered 3 more of Kurt's breakoutboards this summer.
But I do see the advantages of going for a robot with more brain capacity, lol. Like face recognition or SLAM. I'll probably play with both.
Anyway, I've decided to try ROS on one of my next robot projects. Greatly inspired by Kevin's awesome Golem I think its about time to learn something new.
At the moment I've only walked through some of the ROS tutorials. But I think it would be a bit more inspiring to see a live hexapod moving around instead of some turtles on my screen..
So, what hardware do I need? I've noticed some are using the RPI, Odroid or a NUC. It's probably a matter of payload capacity when it comes to a NUC solution like Kevin used. I'm thinking I want to try it on my PhantomX at first. So maybe the Odroid XU4 is a good start?
I believe I need some extra stuff like an eMMC module (16 or 32 GB?). I see they come with preinstalled Xubuntu 15.04, does ROS work fine with that version? Also a bluetooth and wifi USB module. A DC plug cable. I do have an UBEC 5v 8A regulator from Turnigy. Maybe the levelshifter board too? Anything else I've forgot?
At the moment I've several Q's spinning in my head. Like how do you interface with the Odroid? external keyboard, mouse and monitor? How does the main ROS program start by itself, is that the launch files?
Well, I think I need to start at one end.
Bookmarks