Results 1 to 7 of 7

Thread: DC Geared Motor Slow driving

  1. DC Geared Motor Slow driving

    Hi Everyone,

    I am currently working on a undergraduate robotics project, I am tasked to build an autonomous mapping robot.

    I am pretty much finished an d my robot is mapping, but I am struggling with motor control using PWM. I am using a wild thumper chassis with 34:1 geared DC motors, here is a link to the specifications (http://www.communica.co.za/catalog/Details/P4158806527). My motors initial startup voltage is 2V and once running can run slowly below 2V using PWM. I am struggling with the PI controller as I need really slow driving and this initial startup is giving me a problem. Is there anyway using pwm on an arduino based motor controller to achieve slow driving while overcoming the initail voltage. Or any techniques for slow driving with A 34:1 geared DC motor, I know a higher gear ratio will be better for slow driving but I have to do with what I have.

  2. #2

    Re: DC Geared Motor Slow driving

    Is there anyway using pwm on an arduino based motor controller to achieve slow driving while overcoming the initail voltage.
    With PWM, the voltage is always the same, only the duty cycle is different.
    Is it the case that when you say "2V" you really mean a 25% duty cycle, so that a volt meter might show an average of 2V?

    I'm using the Wild Thumper, too, for robomagellan navigation. However, I have modified it to add 34:1 motors with encoders on the two center wheels, this lets me know when the chassis is moving versus not.
    If that's an option for you, that's a fun thing to do!
    (I also use RoboClaw motor controllers that have built-in PID control for driving the motors based on the encoders)

  3. Re: DC Geared Motor Slow driving

    Quote Originally Posted by jwatte View Post
    With PWM, the voltage is always the same, only the duty cycle is different.
    Is it the case that when you say "2V" you really mean a 25% duty cycle, so that a volt meter might show an average of 2V?

    I'm using the Wild Thumper, too, for robomagellan navigation. However, I have modified it to add 34:1 motors with encoders on the two center wheels, this lets me know when the chassis is moving versus not.
    If that's an option for you, that's a fun thing to do!
    (I also use RoboClaw motor controllers that have built-in PID control for driving the motors based on the encoders)
    Yes sorry thats what I meant by 2V. I am using encoders on the centre two wheels, which are working well. The tuning of my PID controller on the other hand is very difficult due to this initial voltage level required. To get it to react fast enough is very difficult.

    My idea is to find out if there is any technique, for instance alternating the PWM signal to a higher level every 50Hz to just to pulse the power to over come this initial torque. The issue is mainly that once the motors are actually going you can easily drive slowly but not from the start.

  4. #4

    Re: DC Geared Motor Slow driving

    Cranking up the "I" term of the PID controller is intended to take care of this, although with that "bump" you will probably then overshoot.

    The best thing I can recommend would be to add another term to the PID controller which is an "impulse response compensator."
    Measure how much "extra oomph" you need to change the speed from standing-still (say, how long does it need to be 100% to break standing still?) and manually add that to the output when you detect that the base speed is "standing still" rather than "moving slowly."
    The trick is to add this compensation after the output of the PID, so that the big oomph isn't "seen" by it and doesn't take the time to "confuse" it.

  5. Re: DC Geared Motor Slow driving

    Quote Originally Posted by jwatte View Post
    Cranking up the "I" term of the PID controller is intended to take care of this, although with that "bump" you will probably then overshoot.

    The best thing I can recommend would be to add another term to the PID controller which is an "impulse response compensator."
    Measure how much "extra oomph" you need to change the speed from standing-still (say, how long does it need to be 100% to break standing still?) and manually add that to the output when you detect that the base speed is "standing still" rather than "moving slowly."
    The trick is to add this compensation after the output of the PID, so that the big oomph isn't "seen" by it and doesn't take the time to "confuse" it.
    Ive tried to ramp up the "I" term but yea i get a lot of overshoot. What difference would the "D" term adjustment have?

    Yea this was the thought in the back of my head, my control systems knowledge is not great so it would entail quite a bit of research. DO you know of any similar implementations that I could use as an example?

  6. #6

    Re: DC Geared Motor Slow driving

    What difference would the "D" term adjustment have?
    It won't really reduce the overshoot, but it will make the system recover smootoher -- not "ring"

    know of any similar implementations that I could use as an example
    At that point you're into nonlinear systems (because the response of the "hump" is nonlinear) and the match is both scary and rather "ad hoc."

    I'd suggest you have a bit of code after your PID controller that simply says this:

    Code:
    if ((actual_speed < SMALL_MINIMUM_SPEED) && (desired_speed > SMALL_MINIMUM_SPEED)) {
        pwm_duty_cycle = max(CONSTANT, pwm_duty_cycle);
    }
    "CONSTANT" could be 100%, or perhaps as low as 30% if that's enough to get over the hump. As soon as the speed is actually bigger than the small-minimum-speed threshold, the "artificial boost" will go away.

  7. Re: DC Geared Motor Slow driving

    Quote Originally Posted by jwatte View Post
    It won't really reduce the overshoot, but it will make the system recover smootoher -- not "ring"



    At that point you're into nonlinear systems (because the response of the "hump" is nonlinear) and the match is both scary and rather "ad hoc."

    I'd suggest you have a bit of code after your PID controller that simply says this:

    Code:
    if ((actual_speed < SMALL_MINIMUM_SPEED) && (desired_speed > SMALL_MINIMUM_SPEED)) {
        pwm_duty_cycle = max(CONSTANT, pwm_duty_cycle);
    }
    "CONSTANT" could be 100%, or perhaps as low as 30% if that's enough to get over the hump. As soon as the speed is actually bigger than the small-minimum-speed threshold, the "artificial boost" will go away.
    Thank you that makes a lot of sense! I will give it a try as soon as I get a chance.

Thread Information

Users Browsing this Thread

There are currently 3 users browsing this thread. (0 members and 3 guests)

Similar Threads

  1. Question(s) How to build a driving, steering, wheel/motor mount?
    By jwatte in forum Mechanics / Construction
    Replies: 12
    Last Post: 02-20-2013, 12:15 PM
  2. Question(s) How do I slow down the motors?
    By ilo_oli in forum Software and Programming
    Replies: 0
    Last Post: 11-01-2011, 06:45 PM
  3. Driving a Solenoid Using the Arbotix
    By sirching in forum DYNAMIXEL & Robot Actuators
    Replies: 0
    Last Post: 03-29-2011, 09:29 PM
  4. Question(s) As Slow As Possible. Seriously.
    By draikani in forum DYNAMIXEL & Robot Actuators
    Replies: 9
    Last Post: 04-18-2010, 02:01 AM
  5. suggestion for small, quiet, slow motor?
    By moodchannel in forum DYNAMIXEL & Robot Actuators
    Replies: 2
    Last Post: 08-07-2009, 12:54 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •